LS1043ARDB unable to boot from SD card with oem image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043ARDB unable to boot from SD card with oem image

549 Views
LSuser
Contributor I

Hi All,

Trying to boot composite image from SD card on LS1043ARDB evaluation board, flashed image ""firmware_ls1043ardb_norboot.img from https://lsdk.github.io,  but boot gets stuck:

Type the escape character to get to the prompt.
VERBOSE: NUM of cluster = 0x1, Cores per cluster = 0x4
INFO: SoC workaround for Errata A008850 Early-Phase was applied
INFO: SoC workaround for Errata A009660 was applied
INFO: SoC workaround for Errata A010539 was applied
INFO: RCW BOOT SRC is SD/EMMC
INFO: SoC workaround for DDR Errata A009942 was applied
INFO: SoC workaround for DDR Errata A009663 was applied
VERBOSE: Generic delay timer configured with mult=1 and div=25
VERBOSE: platform clock 400000000
VERBOSE: DDR PLL1 1600000000
VERBOSE: DDR PLL2 400000000
INFO: time base 13 ms
VERBOSE: Parse DIMM SPD(s)
VERBOSE: cal cs
VERBOSE: cs_in_use = 1
VERBOSE: cs_on_dimm[0] = 1
NOTICE: Fixed DDR on board
INFO: Time after parsing SPD 13 ms
VERBOSE: Synthesize configurations
VERBOSE: cs 0
VERBOSE: odt_rd_cfg 0x0
VERBOSE: odt_wr_cfg 0x4
VERBOSE: odt_rtt_norm 0x3
VERBOSE: odt_rtt_wr 0x0
VERBOSE: auto_precharge 0
VERBOSE: cs 1
VERBOSE: odt_rd_cfg 0x0
VERBOSE: odt_wr_cfg 0x0
VERBOSE: odt_rtt_norm 0x0
VERBOSE: odt_rtt_wr 0x0
VERBOSE: auto_precharge 0
VERBOSE: cs 2
VERBOSE: odt_rd_cfg 0x0
VERBOSE: odt_wr_cfg 0x0
VERBOSE: odt_rtt_norm 0x0
VERBOSE: odt_rtt_wr 0x0
VERBOSE: auto_precharge 0
VERBOSE: cs 3
VERBOSE: odt_rd_cfg 0x0
VERBOSE: odt_wr_cfg 0x0
VERBOSE: odt_rtt_norm 0x0
VERBOSE: odt_rtt_wr 0x0
VERBOSE: auto_precharge 0
VERBOSE: ctlr_init_ecc 0
VERBOSE: x4_en 0
VERBOSE: ap_en 0
VERBOSE: ctlr_intlv 0
VERBOSE: ctlr_intlv_mode 0
VERBOSE: ba_intlv 0x0
VERBOSE: data_bus_used 1
VERBOSE: otf_burst_chop_en 0
VERBOSE: burst_length 0x8
VERBOSE: dbw_cap_shift 0
VERBOSE: Assign binding addresses
VERBOSE: ctlr_intlv 0
VERBOSE: rank density 0x80000000
VERBOSE: CS 0
VERBOSE: base_addr 0x0
VERBOSE: size 0x80000000
VERBOSE: base 0x0
VERBOSE: Total mem by assignment is 0x80000000
VERBOSE: Calculate controller registers
VERBOSE: Skip CL mask for this speed 0x0
VERBOSE: Skip caslat 0x0
VERBOSE: cs_in_use = 0x1
VERBOSE: cs0
VERBOSE: _config = 0x80040322
VERBOSE: cs[0].bnds = 0x7f
VERBOSE: sdram_cfg[0] = 0xc50c0000
VERBOSE: sdram_cfg[1] = 0x401100
VERBOSE: sdram_cfg[2] = 0x0
VERBOSE: timing_cfg[0] = 0x91550018
VERBOSE: timing_cfg[1] = 0xbbb48c42
VERBOSE: timing_cfg[2] = 0x48c111
VERBOSE: timing_cfg[3] = 0x10c1000
VERBOSE: timing_cfg[4] = 0x2
VERBOSE: timing_cfg[5] = 0x3401400
VERBOSE: timing_cfg[6] = 0x0
VERBOSE: timing_cfg[7] = 0x13300000
VERBOSE: timing_cfg[8] = 0x2115600
VERBOSE: timing_cfg[9] = 0x0
VERBOSE: dq_map[0] = 0x0
VERBOSE: dq_map[1] = 0x0
VERBOSE: dq_map[2] = 0x0
VERBOSE: dq_map[3] = 0x0
VERBOSE: sdram_mode[0] = 0x3010210
VERBOSE: sdram_mode[1] = 0x0
VERBOSE: sdram_mode[9] = 0x4000000
VERBOSE: sdram_mode[8] = 0x500
VERBOSE: sdram_mode[2] = 0x10210
VERBOSE: sdram_mode[3] = 0x0
VERBOSE: sdram_mode[10] = 0x400
VERBOSE: sdram_mode[11] = 0x4000000
VERBOSE: sdram_mode[4] = 0x10210
VERBOSE: sdram_mode[5] = 0x0
VERBOSE: sdram_mode[12] = 0x400
VERBOSE: sdram_mode[13] = 0x4000000
VERBOSE: sdram_mode[6] = 0x10210
VERBOSE: sdram_mode[7] = 0x0
VERBOSE: sdram_mode[14] = 0x400
VERBOSE: sdram_mode[15] = 0x4000000
VERBOSE: interval = 0x18600618
VERBOSE: zq_cntl = 0x8a090705
VERBOSE: ddr_sr_cntr = 0x0
VERBOSE: clk_cntl = 0x3000000
VERBOSE: cdr[0] = 0x80040000
VERBOSE: cdr[1] = 0xa181
VERBOSE: wrlvl_cntl[0] = 0x8675f607
VERBOSE: wrlvl_cntl[1] = 0x7090807
VERBOSE: wrlvl_cntl[2] = 0x7070707
VERBOSE: debug[28] = 0x46
INFO: Time before programming controller 260 ms
VERBOSE: Program controller registers
VERBOSE: Reading debug[9] as 0x10101010
VERBOSE: Reading debug[10] as 0x10101010
VERBOSE: cpo_min 0x10
VERBOSE: cpo_max 0x10
VERBOSE: debug[28] 0x700046
VERBOSE: Optimal cpo_sample 0x37

NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off
INFO: Time used by DDR driver 690 ms
INFO: SoC workaround for Errata A008850 Post-Phase was applied
INFO: RCW BOOT SRC is SD/EMMC
INFO: esdhc_emmc_init
INFO: Card detected successfully
INFO: init done:
VERBOSE: Memory seen by this BL image: 0x10000000 - 0x10015000
VERBOSE: Code region: 0x10000000 - 0x10009000
VERBOSE: Read-only data region: 0x10009000 - 0x1000c000
VERBOSE: DRAM Region 0: 0x80000000 - 0xfbdfffff
VERBOSE: Secure DRAM Region 0: 0xfbe00000 - 0xffffffff
mmap:
VA:0x1000000 PA:0x1000000 size:0xf000000 attr:0x8 granularity:0x40000000
VA:0x10000000 PA:0x10000000 size:0x9000 attr:0x2 granularity:0x40000000
VA:0x10009000 PA:0x10009000 size:0x3000 attr:0x22 granularity:0x40000000
VA:0x10000000 PA:0x10000000 size:0x15000 attr:0xa granularity:0x40000000
VA:0x80000000 PA:0x80000000 size:0x7be00000 attr:0x1a granularity:0x40000000
VA:0xfbe00000 PA:0xfbe00000 size:0x4200000 attr:0xa granularity:0x40000000

VERBOSE: Translation tables state:
VERBOSE: Xlat regime: EL3
VERBOSE: Max allowed PA: 0xffffffffff
VERBOSE: Max allowed VA: 0xffffffffff
VERBOSE: Max mapped PA: 0xffffffff
VERBOSE: Max mapped VA: 0xffffffff
VERBOSE: Initial lookup level: 0
VERBOSE: Entries @initial lookup level: 2
VERBOSE: Used 4 sub-tables out of 6 (spare: 2)
[LV0] VA:0x0 size:0x8000000000
[LV1] VA:0x0 size:0x40000000
[LV2] VA:0x0 size:0x200000
[LV2] (7 invalid descriptors omitted)
[LV2] VA:0x1000000 PA:0x1000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x1200000 PA:0x1200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x1400000 PA:0x1400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x1600000 PA:0x1600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x1800000 PA:0x1800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x1a00000 PA:0x1a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x1c00000 PA:0x1c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x1e00000 PA:0x1e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2000000 PA:0x2000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2200000 PA:0x2200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2400000 PA:0x2400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2600000 PA:0x2600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2800000 PA:0x2800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2a00000 PA:0x2a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2c00000 PA:0x2c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x2e00000 PA:0x2e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3000000 PA:0x3000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3200000 PA:0x3200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3400000 PA:0x3400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3600000 PA:0x3600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3800000 PA:0x3800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3a00000 PA:0x3a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3c00000 PA:0x3c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x3e00000 PA:0x3e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4000000 PA:0x4000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4200000 PA:0x4200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4400000 PA:0x4400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4600000 PA:0x4600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4800000 PA:0x4800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4a00000 PA:0x4a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4c00000 PA:0x4c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x4e00000 PA:0x4e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5000000 PA:0x5000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5200000 PA:0x5200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5400000 PA:0x5400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5600000 PA:0x5600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5800000 PA:0x5800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5a00000 PA:0x5a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5c00000 PA:0x5c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x5e00000 PA:0x5e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6000000 PA:0x6000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6200000 PA:0x6200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6400000 PA:0x6400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6600000 PA:0x6600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6800000 PA:0x6800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6a00000 PA:0x6a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6c00000 PA:0x6c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x6e00000 PA:0x6e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7000000 PA:0x7000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7200000 PA:0x7200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7400000 PA:0x7400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7600000 PA:0x7600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7800000 PA:0x7800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7a00000 PA:0x7a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7c00000 PA:0x7c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x7e00000 PA:0x7e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8000000 PA:0x8000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8200000 PA:0x8200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8400000 PA:0x8400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8600000 PA:0x8600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8800000 PA:0x8800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8a00000 PA:0x8a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8c00000 PA:0x8c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x8e00000 PA:0x8e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9000000 PA:0x9000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9200000 PA:0x9200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9400000 PA:0x9400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9600000 PA:0x9600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9800000 PA:0x9800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9a00000 PA:0x9a00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9c00000 PA:0x9c00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x9e00000 PA:0x9e00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xa000000 PA:0xa000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xa200000 PA:0xa200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xa400000 PA:0xa400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xa600000 PA:0xa600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xa800000 PA:0xa800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xaa00000 PA:0xaa00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xac00000 PA:0xac00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xae00000 PA:0xae00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xb000000 PA:0xb000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xb200000 PA:0xb200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xb400000 PA:0xb400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xb600000 PA:0xb600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xb800000 PA:0xb800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xba00000 PA:0xba00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xbc00000 PA:0xbc00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xbe00000 PA:0xbe00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xc000000 PA:0xc000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xc200000 PA:0xc200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xc400000 PA:0xc400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xc600000 PA:0xc600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xc800000 PA:0xc800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xca00000 PA:0xca00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xcc00000 PA:0xcc00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xce00000 PA:0xce00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xd000000 PA:0xd000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xd200000 PA:0xd200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xd400000 PA:0xd400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xd600000 PA:0xd600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xd800000 PA:0xd800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xda00000 PA:0xda00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xdc00000 PA:0xdc00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xde00000 PA:0xde00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xe000000 PA:0xe000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xe200000 PA:0xe200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xe400000 PA:0xe400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xe600000 PA:0xe600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xe800000 PA:0xe800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xea00000 PA:0xea00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xec00000 PA:0xec00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xee00000 PA:0xee00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xf000000 PA:0xf000000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xf200000 PA:0xf200000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xf400000 PA:0xf400000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xf600000 PA:0xf600000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xf800000 PA:0xf800000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xfa00000 PA:0xfa00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xfc00000 PA:0xfc00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0xfe00000 PA:0xfe00000 size:0x200000 DEV-RW-XN-S
[LV2] VA:0x10000000 size:0x200000
[LV3] VA:0x10000000 PA:0x10000000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10001000 PA:0x10001000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10002000 PA:0x10002000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10003000 PA:0x10003000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10004000 PA:0x10004000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10005000 PA:0x10005000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10006000 PA:0x10006000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10007000 PA:0x10007000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10008000 PA:0x10008000 size:0x1000 MEM-RO-EXEC-S
[LV3] VA:0x10009000 PA:0x10009000 size:0x1000 MEM-RO-XN-S
[LV3] VA:0x1000a000 PA:0x1000a000 size:0x1000 MEM-RO-XN-S
[LV3] VA:0x1000b000 PA:0x1000b000 size:0x1000 MEM-RO-XN-S
[LV3] VA:0x1000c000 PA:0x1000c000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x1000d000 PA:0x1000d000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x1000e000 PA:0x1000e000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x1000f000 PA:0x1000f000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x10010000 PA:0x10010000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x10011000 PA:0x10011000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x10012000 PA:0x10012000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x10013000 PA:0x10013000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x10014000 PA:0x10014000 size:0x1000 MEM-RW-XN-S
[LV3] VA:0x10015000 size:0x1000
[LV3] (490 invalid descriptors omitted)
[LV2] VA:0x10200000 size:0x200000
[LV2] (382 invalid descriptors omitted)
[LV1] VA:0x40000000 size:0x40000000
[LV1] VA:0x80000000 PA:0x80000000 size:0x40000000 MEM-RW-XN-NS
[LV1] VA:0xc0000000 size:0x40000000
[LV2] VA:0xc0000000 PA:0xc0000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc0200000 PA:0xc0200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc0400000 PA:0xc0400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc0600000 PA:0xc0600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc0800000 PA:0xc0800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc0a00000 PA:0xc0a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc0c00000 PA:0xc0c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc0e00000 PA:0xc0e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1000000 PA:0xc1000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1200000 PA:0xc1200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1400000 PA:0xc1400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1600000 PA:0xc1600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1800000 PA:0xc1800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1a00000 PA:0xc1a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1c00000 PA:0xc1c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc1e00000 PA:0xc1e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2000000 PA:0xc2000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2200000 PA:0xc2200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2400000 PA:0xc2400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2600000 PA:0xc2600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2800000 PA:0xc2800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2a00000 PA:0xc2a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2c00000 PA:0xc2c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc2e00000 PA:0xc2e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3000000 PA:0xc3000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3200000 PA:0xc3200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3400000 PA:0xc3400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3600000 PA:0xc3600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3800000 PA:0xc3800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3a00000 PA:0xc3a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3c00000 PA:0xc3c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc3e00000 PA:0xc3e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4000000 PA:0xc4000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4200000 PA:0xc4200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4400000 PA:0xc4400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4600000 PA:0xc4600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4800000 PA:0xc4800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4a00000 PA:0xc4a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4c00000 PA:0xc4c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc4e00000 PA:0xc4e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5000000 PA:0xc5000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5200000 PA:0xc5200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5400000 PA:0xc5400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5600000 PA:0xc5600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5800000 PA:0xc5800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5a00000 PA:0xc5a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5c00000 PA:0xc5c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc5e00000 PA:0xc5e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6000000 PA:0xc6000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6200000 PA:0xc6200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6400000 PA:0xc6400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6600000 PA:0xc6600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6800000 PA:0xc6800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6a00000 PA:0xc6a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6c00000 PA:0xc6c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc6e00000 PA:0xc6e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7000000 PA:0xc7000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7200000 PA:0xc7200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7400000 PA:0xc7400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7600000 PA:0xc7600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7800000 PA:0xc7800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7a00000 PA:0xc7a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7c00000 PA:0xc7c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc7e00000 PA:0xc7e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8000000 PA:0xc8000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8200000 PA:0xc8200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8400000 PA:0xc8400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8600000 PA:0xc8600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8800000 PA:0xc8800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8a00000 PA:0xc8a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8c00000 PA:0xc8c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc8e00000 PA:0xc8e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9000000 PA:0xc9000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9200000 PA:0xc9200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9400000 PA:0xc9400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9600000 PA:0xc9600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9800000 PA:0xc9800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9a00000 PA:0xc9a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9c00000 PA:0xc9c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xc9e00000 PA:0xc9e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xca000000 PA:0xca000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xca200000 PA:0xca200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xca400000 PA:0xca400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xca600000 PA:0xca600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xca800000 PA:0xca800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcaa00000 PA:0xcaa00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcac00000 PA:0xcac00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcae00000 PA:0xcae00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcb000000 PA:0xcb000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcb200000 PA:0xcb200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcb400000 PA:0xcb400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcb600000 PA:0xcb600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcb800000 PA:0xcb800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcba00000 PA:0xcba00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcbc00000 PA:0xcbc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcbe00000 PA:0xcbe00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcc000000 PA:0xcc000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcc200000 PA:0xcc200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcc400000 PA:0xcc400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcc600000 PA:0xcc600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcc800000 PA:0xcc800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcca00000 PA:0xcca00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xccc00000 PA:0xccc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcce00000 PA:0xcce00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcd000000 PA:0xcd000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcd200000 PA:0xcd200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcd400000 PA:0xcd400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcd600000 PA:0xcd600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcd800000 PA:0xcd800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcda00000 PA:0xcda00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcdc00000 PA:0xcdc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcde00000 PA:0xcde00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xce000000 PA:0xce000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xce200000 PA:0xce200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xce400000 PA:0xce400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xce600000 PA:0xce600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xce800000 PA:0xce800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcea00000 PA:0xcea00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcec00000 PA:0xcec00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcee00000 PA:0xcee00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcf000000 PA:0xcf000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcf200000 PA:0xcf200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcf400000 PA:0xcf400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcf600000 PA:0xcf600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcf800000 PA:0xcf800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcfa00000 PA:0xcfa00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcfc00000 PA:0xcfc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xcfe00000 PA:0xcfe00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0000000 PA:0xd0000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0200000 PA:0xd0200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0400000 PA:0xd0400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0600000 PA:0xd0600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0800000 PA:0xd0800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0a00000 PA:0xd0a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0c00000 PA:0xd0c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd0e00000 PA:0xd0e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1000000 PA:0xd1000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1200000 PA:0xd1200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1400000 PA:0xd1400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1600000 PA:0xd1600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1800000 PA:0xd1800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1a00000 PA:0xd1a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1c00000 PA:0xd1c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd1e00000 PA:0xd1e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2000000 PA:0xd2000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2200000 PA:0xd2200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2400000 PA:0xd2400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2600000 PA:0xd2600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2800000 PA:0xd2800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2a00000 PA:0xd2a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2c00000 PA:0xd2c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd2e00000 PA:0xd2e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3000000 PA:0xd3000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3200000 PA:0xd3200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3400000 PA:0xd3400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3600000 PA:0xd3600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3800000 PA:0xd3800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3a00000 PA:0xd3a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3c00000 PA:0xd3c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd3e00000 PA:0xd3e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4000000 PA:0xd4000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4200000 PA:0xd4200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4400000 PA:0xd4400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4600000 PA:0xd4600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4800000 PA:0xd4800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4a00000 PA:0xd4a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4c00000 PA:0xd4c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd4e00000 PA:0xd4e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5000000 PA:0xd5000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5200000 PA:0xd5200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5400000 PA:0xd5400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5600000 PA:0xd5600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5800000 PA:0xd5800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5a00000 PA:0xd5a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5c00000 PA:0xd5c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd5e00000 PA:0xd5e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6000000 PA:0xd6000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6200000 PA:0xd6200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6400000 PA:0xd6400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6600000 PA:0xd6600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6800000 PA:0xd6800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6a00000 PA:0xd6a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6c00000 PA:0xd6c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd6e00000 PA:0xd6e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7000000 PA:0xd7000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7200000 PA:0xd7200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7400000 PA:0xd7400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7600000 PA:0xd7600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7800000 PA:0xd7800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7a00000 PA:0xd7a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7c00000 PA:0xd7c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd7e00000 PA:0xd7e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8000000 PA:0xd8000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8200000 PA:0xd8200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8400000 PA:0xd8400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8600000 PA:0xd8600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8800000 PA:0xd8800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8a00000 PA:0xd8a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8c00000 PA:0xd8c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd8e00000 PA:0xd8e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9000000 PA:0xd9000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9200000 PA:0xd9200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9400000 PA:0xd9400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9600000 PA:0xd9600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9800000 PA:0xd9800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9a00000 PA:0xd9a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9c00000 PA:0xd9c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xd9e00000 PA:0xd9e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xda000000 PA:0xda000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xda200000 PA:0xda200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xda400000 PA:0xda400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xda600000 PA:0xda600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xda800000 PA:0xda800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdaa00000 PA:0xdaa00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdac00000 PA:0xdac00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdae00000 PA:0xdae00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdb000000 PA:0xdb000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdb200000 PA:0xdb200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdb400000 PA:0xdb400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdb600000 PA:0xdb600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdb800000 PA:0xdb800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdba00000 PA:0xdba00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdbc00000 PA:0xdbc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdbe00000 PA:0xdbe00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdc000000 PA:0xdc000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdc200000 PA:0xdc200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdc400000 PA:0xdc400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdc600000 PA:0xdc600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdc800000 PA:0xdc800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdca00000 PA:0xdca00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdcc00000 PA:0xdcc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdce00000 PA:0xdce00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdd000000 PA:0xdd000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdd200000 PA:0xdd200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdd400000 PA:0xdd400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdd600000 PA:0xdd600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdd800000 PA:0xdd800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdda00000 PA:0xdda00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xddc00000 PA:0xddc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdde00000 PA:0xdde00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xde000000 PA:0xde000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xde200000 PA:0xde200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xde400000 PA:0xde400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xde600000 PA:0xde600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xde800000 PA:0xde800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdea00000 PA:0xdea00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdec00000 PA:0xdec00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdee00000 PA:0xdee00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdf000000 PA:0xdf000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdf200000 PA:0xdf200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdf400000 PA:0xdf400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdf600000 PA:0xdf600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdf800000 PA:0xdf800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdfa00000 PA:0xdfa00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdfc00000 PA:0xdfc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xdfe00000 PA:0xdfe00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0000000 PA:0xe0000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0200000 PA:0xe0200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0400000 PA:0xe0400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0600000 PA:0xe0600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0800000 PA:0xe0800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0a00000 PA:0xe0a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0c00000 PA:0xe0c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe0e00000 PA:0xe0e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1000000 PA:0xe1000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1200000 PA:0xe1200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1400000 PA:0xe1400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1600000 PA:0xe1600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1800000 PA:0xe1800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1a00000 PA:0xe1a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1c00000 PA:0xe1c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe1e00000 PA:0xe1e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2000000 PA:0xe2000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2200000 PA:0xe2200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2400000 PA:0xe2400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2600000 PA:0xe2600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2800000 PA:0xe2800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2a00000 PA:0xe2a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2c00000 PA:0xe2c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe2e00000 PA:0xe2e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3000000 PA:0xe3000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3200000 PA:0xe3200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3400000 PA:0xe3400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3600000 PA:0xe3600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3800000 PA:0xe3800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3a00000 PA:0xe3a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3c00000 PA:0xe3c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe3e00000 PA:0xe3e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4000000 PA:0xe4000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4200000 PA:0xe4200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4400000 PA:0xe4400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4600000 PA:0xe4600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4800000 PA:0xe4800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4a00000 PA:0xe4a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4c00000 PA:0xe4c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe4e00000 PA:0xe4e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5000000 PA:0xe5000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5200000 PA:0xe5200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5400000 PA:0xe5400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5600000 PA:0xe5600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5800000 PA:0xe5800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5a00000 PA:0xe5a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5c00000 PA:0xe5c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe5e00000 PA:0xe5e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6000000 PA:0xe6000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6200000 PA:0xe6200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6400000 PA:0xe6400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6600000 PA:0xe6600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6800000 PA:0xe6800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6a00000 PA:0xe6a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6c00000 PA:0xe6c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe6e00000 PA:0xe6e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7000000 PA:0xe7000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7200000 PA:0xe7200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7400000 PA:0xe7400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7600000 PA:0xe7600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7800000 PA:0xe7800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7a00000 PA:0xe7a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7c00000 PA:0xe7c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe7e00000 PA:0xe7e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8000000 PA:0xe8000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8200000 PA:0xe8200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8400000 PA:0xe8400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8600000 PA:0xe8600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8800000 PA:0xe8800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8a00000 PA:0xe8a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8c00000 PA:0xe8c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe8e00000 PA:0xe8e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9000000 PA:0xe9000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9200000 PA:0xe9200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9400000 PA:0xe9400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9600000 PA:0xe9600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9800000 PA:0xe9800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9a00000 PA:0xe9a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9c00000 PA:0xe9c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xe9e00000 PA:0xe9e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xea000000 PA:0xea000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xea200000 PA:0xea200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xea400000 PA:0xea400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xea600000 PA:0xea600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xea800000 PA:0xea800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeaa00000 PA:0xeaa00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeac00000 PA:0xeac00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeae00000 PA:0xeae00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeb000000 PA:0xeb000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeb200000 PA:0xeb200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeb400000 PA:0xeb400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeb600000 PA:0xeb600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeb800000 PA:0xeb800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeba00000 PA:0xeba00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xebc00000 PA:0xebc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xebe00000 PA:0xebe00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xec000000 PA:0xec000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xec200000 PA:0xec200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xec400000 PA:0xec400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xec600000 PA:0xec600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xec800000 PA:0xec800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeca00000 PA:0xeca00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xecc00000 PA:0xecc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xece00000 PA:0xece00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xed000000 PA:0xed000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xed200000 PA:0xed200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xed400000 PA:0xed400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xed600000 PA:0xed600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xed800000 PA:0xed800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeda00000 PA:0xeda00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xedc00000 PA:0xedc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xede00000 PA:0xede00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xee000000 PA:0xee000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xee200000 PA:0xee200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xee400000 PA:0xee400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xee600000 PA:0xee600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xee800000 PA:0xee800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeea00000 PA:0xeea00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeec00000 PA:0xeec00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xeee00000 PA:0xeee00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xef000000 PA:0xef000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xef200000 PA:0xef200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xef400000 PA:0xef400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xef600000 PA:0xef600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xef800000 PA:0xef800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xefa00000 PA:0xefa00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xefc00000 PA:0xefc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xefe00000 PA:0xefe00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0000000 PA:0xf0000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0200000 PA:0xf0200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0400000 PA:0xf0400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0600000 PA:0xf0600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0800000 PA:0xf0800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0a00000 PA:0xf0a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0c00000 PA:0xf0c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf0e00000 PA:0xf0e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1000000 PA:0xf1000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1200000 PA:0xf1200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1400000 PA:0xf1400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1600000 PA:0xf1600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1800000 PA:0xf1800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1a00000 PA:0xf1a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1c00000 PA:0xf1c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf1e00000 PA:0xf1e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2000000 PA:0xf2000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2200000 PA:0xf2200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2400000 PA:0xf2400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2600000 PA:0xf2600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2800000 PA:0xf2800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2a00000 PA:0xf2a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2c00000 PA:0xf2c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf2e00000 PA:0xf2e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3000000 PA:0xf3000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3200000 PA:0xf3200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3400000 PA:0xf3400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3600000 PA:0xf3600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3800000 PA:0xf3800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3a00000 PA:0xf3a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3c00000 PA:0xf3c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf3e00000 PA:0xf3e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4000000 PA:0xf4000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4200000 PA:0xf4200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4400000 PA:0xf4400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4600000 PA:0xf4600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4800000 PA:0xf4800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4a00000 PA:0xf4a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4c00000 PA:0xf4c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf4e00000 PA:0xf4e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5000000 PA:0xf5000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5200000 PA:0xf5200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5400000 PA:0xf5400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5600000 PA:0xf5600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5800000 PA:0xf5800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5a00000 PA:0xf5a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5c00000 PA:0xf5c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf5e00000 PA:0xf5e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6000000 PA:0xf6000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6200000 PA:0xf6200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6400000 PA:0xf6400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6600000 PA:0xf6600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6800000 PA:0xf6800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6a00000 PA:0xf6a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6c00000 PA:0xf6c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf6e00000 PA:0xf6e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7000000 PA:0xf7000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7200000 PA:0xf7200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7400000 PA:0xf7400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7600000 PA:0xf7600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7800000 PA:0xf7800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7a00000 PA:0xf7a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7c00000 PA:0xf7c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf7e00000 PA:0xf7e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8000000 PA:0xf8000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8200000 PA:0xf8200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8400000 PA:0xf8400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8600000 PA:0xf8600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8800000 PA:0xf8800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8a00000 PA:0xf8a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8c00000 PA:0xf8c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf8e00000 PA:0xf8e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9000000 PA:0xf9000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9200000 PA:0xf9200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9400000 PA:0xf9400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9600000 PA:0xf9600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9800000 PA:0xf9800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9a00000 PA:0xf9a00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9c00000 PA:0xf9c00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xf9e00000 PA:0xf9e00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfa000000 PA:0xfa000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfa200000 PA:0xfa200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfa400000 PA:0xfa400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfa600000 PA:0xfa600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfa800000 PA:0xfa800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfaa00000 PA:0xfaa00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfac00000 PA:0xfac00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfae00000 PA:0xfae00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfb000000 PA:0xfb000000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfb200000 PA:0xfb200000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfb400000 PA:0xfb400000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfb600000 PA:0xfb600000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfb800000 PA:0xfb800000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfba00000 PA:0xfba00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfbc00000 PA:0xfbc00000 size:0x200000 MEM-RW-XN-NS
[LV2] VA:0xfbe00000 PA:0xfbe00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfc000000 PA:0xfc000000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfc200000 PA:0xfc200000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfc400000 PA:0xfc400000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfc600000 PA:0xfc600000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfc800000 PA:0xfc800000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfca00000 PA:0xfca00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfcc00000 PA:0xfcc00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfce00000 PA:0xfce00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfd000000 PA:0xfd000000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfd200000 PA:0xfd200000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfd400000 PA:0xfd400000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfd600000 PA:0xfd600000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfd800000 PA:0xfd800000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfda00000 PA:0xfda00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfdc00000 PA:0xfdc00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfde00000 PA:0xfde00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfe000000 PA:0xfe000000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfe200000 PA:0xfe200000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfe400000 PA:0xfe400000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfe600000 PA:0xfe600000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfe800000 PA:0xfe800000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfea00000 PA:0xfea00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfec00000 PA:0xfec00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xfee00000 PA:0xfee00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xff000000 PA:0xff000000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xff200000 PA:0xff200000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xff400000 PA:0xff400000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xff600000 PA:0xff600000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xff800000 PA:0xff800000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xffa00000 PA:0xffa00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xffc00000 PA:0xffc00000 size:0x200000 MEM-RW-XN-S
[LV2] VA:0xffe00000 PA:0xffe00000 size:0x200000 MEM-RW-XN-S
[LV1] VA:0x100000000 size:0x40000000
[LV1] (507 invalid descriptors omitted)
[LV0] VA:0x8000000000 size:0x8000000000
NOTICE: BL2: v2.4(release):LSDK-21.08-0-g340b20bcb-dirty
NOTICE: BL2: Built : 08:17:00, Jul 16 2024
INFO: Configuring TrustZone Controller tzc380
INFO: BL2: Doing platform setup
INFO: BL2: Loading image id 3
INFO: sd-mmc read done.

Any ideas what could be wrong ?

0 Kudos
Reply
5 Replies

519 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

It seems that you've flashed the wrong image, you are booting from sd with the image "firmware_ls1043ardb_norboot.img", please try again with the corresponding image for sd:

firmware_ls1043ardb_sdboot.img

Have a nice day!

 

0 Kudos
Reply

506 Views
LSuser
Contributor I

Sorry, I copied the wrong image name to this post. I have double checked and it was sd image that was flashed: firmware_ls1043ardb_sdboot.img to the SD, and the output was with this image. Is there any way to debug this ?

0 Kudos
Reply

501 Views
Oswalag
NXP TechSupport
NXP TechSupport

Please share the process you followed to flash the firmware and also please share your switch settings on board. 

0 Kudos
Reply

466 Views
LSuser
Contributor I
I have tried various ways to flash firmware, the last one was " flex-installer -i auto -m ls1043ardb -d /dev/mmcblk0".

But results are the same, boot is stuck:



NOTICE: Fixed DDR on board



NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off

NOTICE: BL2: v2.4(release):LSDK-21.08-0-g340b20bcb

NOTICE: BL2: Built : 22:20:23, Aug 27 2021



DIP jumpers configuration:



SW3 - 10010011



SW4 - 00100000



SW5 - 00100010

0 Kudos
Reply

466 Views
LSuser
Contributor I

Hi,
I have tried various ways to flash composite image, the last was "flex-installer -i auto -m ls1043ardb -d /dev/mmcblk0", and results are the same, boot is stuck at:

NOTICE: Fixed DDR on board

NOTICE: 2 GB DDR4, 32-bit, CL=11, ECC off
NOTICE: BL2: v2.4(release):LSDK-21.08-0-g340b20bcb
NOTICE: BL2: Built : 22:20:23, Aug 27 2021

DIP Switches configurations are the following:

SW3 - 10010011
SW4 - 00100000
SW5 - 00100010

0 Kudos
Reply