LS1028 PTP4L eno0 port cause link down linkup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1028 PTP4L eno0 port cause link down linkup

619 次查看
xinliwang
Contributor III

Hi @kenli 

I found when running "ptp4l -i eno0 -f  gptp.cfg -m" at the first time. It shows port link down and up. 

xinliwang_0-1687833608129.png

But when I use switch port swp0, it would not cause the link down/up problem.

 

If we run an eth application before time sync(ptp4l -i eno0 -f  gptp.cfg), it will cause the port link down which is not allowed.

So I have two questions down below:

1. Why it is different between eno0 and swp0 by using the same ptp4l command?

2. How do I avoid such link up/down problem on eno0 port? 

Thanks

标记 (1)
0 项奖励
回复
2 回复数

599 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "8.8.1.3 Basic TSN configuration examples on ENETC" in LSDKUG_Rev21.08.pdf

0 项奖励
回复

585 次查看
xinliwang
Contributor III

Hi @yipingwang 

Thank you for your reply.

I could not find solution from the file, but I think it is the ptp4l strategy.Maybe it is better to post my question on PTP forum.

Thank you

0 项奖励
回复