LS1028 PTP4L eno0 port cause link down linkup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1028 PTP4L eno0 port cause link down linkup

616件の閲覧回数
xinliwang
Contributor III

Hi @kenli 

I found when running "ptp4l -i eno0 -f  gptp.cfg -m" at the first time. It shows port link down and up. 

xinliwang_0-1687833608129.png

But when I use switch port swp0, it would not cause the link down/up problem.

 

If we run an eth application before time sync(ptp4l -i eno0 -f  gptp.cfg), it will cause the port link down which is not allowed.

So I have two questions down below:

1. Why it is different between eno0 and swp0 by using the same ptp4l command?

2. How do I avoid such link up/down problem on eno0 port? 

Thanks

タグ(1)
0 件の賞賛
返信
2 返答(返信)

596件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "8.8.1.3 Basic TSN configuration examples on ENETC" in LSDKUG_Rev21.08.pdf

0 件の賞賛
返信

582件の閲覧回数
xinliwang
Contributor III

Hi @yipingwang 

Thank you for your reply.

I could not find solution from the file, but I think it is the ptp4l strategy.Maybe it is better to post my question on PTP forum.

Thank you

0 件の賞賛
返信