LS1021A PLL setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LS1021A PLL setting

1,951 次查看
deepaknaiknavar
Contributor II

Hi,

I am evaluating LS1021A for one of our project.

Does code warrior provide option of performing PLL settings for all interfaces like DDRclk, Sysclk etc.?

I see SerDes Configuration and Validation is the tool for the same. If yes, then is it free or do we need to purchase it?

Thanks,

Deepak.

标签 (1)
标记 (1)
6 回复数

1,849 次查看
pranavmadhu
Contributor IV

Hi Deepak,

You have to download 'CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA' to modify clock settings from reset configuration word(RCW). You can modify PLL config in RCW using the codewarrior tool. For more details about codewarrior tool refer

CodeWarrior ARMv8 64 bit |NXP

http://www.nxp.com/files/soft_dev_tools/doc/fact_sheet/LSARMv8ISAFS.pdf?fasp=1&WT_TYPE=Fact%20Sheets...

0 项奖励
回复

1,849 次查看
ufedor
NXP Employee
NXP Employee

> You have to download 'CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA'

This statement is not correct because LS1021A belongs to ARMv7.

0 项奖励
回复

1,849 次查看
pranavmadhu
Contributor IV

Hi Ufedor,

Thank you for correcting me. I'm having ubuntu 12.04 machine. I've attached a screen shot of the code warrior tool that I use. temp.png

In this it is displayed that ARM V8 ISA, and the pbl generated for qspi using this version works for my LS1021A-IOT board.

0 项奖励
回复

1,849 次查看
ufedor
NXP Employee
NXP Employee

The same QCVS is used by ARMv7 and ARMv8 CodeWarrior IDEs.

1,849 次查看
deepaknaiknavar
Contributor II

Thanks Ufedor and Pranav,

0 项奖励
回复

1,849 次查看
ufedor
NXP Employee
NXP Employee

The request is not clear - is it about RCW preparation?

0 项奖励
回复