Hi,
Did full build "flex-builder -m ls1012ardb -b qspi" and got all images created then flashed on my RDB.
Boots well, nor problems. Boot partition and RFS user land are on a USB stick, all ok.
Below my output:
My problem now is (maybe stupid but tried and searched but no success yet) that I arrive into the login screen and there am asked for:
NXP LSDK 1909 main
localhost login:
Tried several things but cannot log into it. What are the credentials? Was also looking in sources and Community here but cannot find it.
Thx Christophe
解決済! 解決策の投稿を見る。
Update. Finally did a complete rebuild and reflash, possible I'd some mess in my files somewhere, whatever ...
Also you must understand I did the scp move to bring in tarballs on my sda3 from outside and not from inside the target seeing my network infrastructure - so I had an open SCP session into my target from outside (that worked fine). Think I've to close this session first then reboot and all works with root/root credentials. Keeping the outside SCP session active while rebooting does not work - and make sense. Agree? Thx Christophe
Update. Finally did a complete rebuild and reflash, possible I'd some mess in my files somewhere, whatever ...
Also you must understand I did the scp move to bring in tarballs on my sda3 from outside and not from inside the target seeing my network infrastructure - so I had an open SCP session into my target from outside (that worked fine). Think I've to close this session first then reboot and all works with root/root credentials. Keeping the outside SCP session active while rebooting does not work - and make sense. Agree? Thx Christophe
Use "root" as login & password
Yep, did this already: root/root, root/toor, user/user, user/(no pwd), root/(no pwd), (no user)/(no pwd) etc.
Says all the time Login incorrect. Also login times out after 60 sec. if doing nothing.
You wrote:
> Boot partition and RFS user land are on a USB stick
What is the origin of the stick?
Please provide complete U-Boot + Linux textual booting logs as attachments.
Sorry - where did yo get the stick?
Was it made using the LSDK 1909 components?
I am not sure to understand. When you say where you mean where I bought it?? Sounds weird but maybe just a misunderstanding please reformulate again.
In many reported use cases I see that login is "root" and password is empty.
Was the stick made by you using the LSDK 1909 components?
I was relying myself on document "LS1012ARDBGSG.pdf", rev5 8/2018, a following especially the chapter "§14 Deploying Ubuntu userland on LS1012ARDB".
My aim is to be able to fully build firmware (that seems to works) and the boot partition + RFS (which must be put on USB stick in my case indeed).
To answer your question: yes I prepped the stick following instructions given in "§14.5.2 Option 2: By preparing SDHC card on the board". I did it the target way via udhcpc method. So yes I used flex-installer as explained expect my device was not /dev/mmcblk0 but /dev/sda. At the end I got also four partitions and enterer 3rd partition (think labelled "backup") where I put both tarballs coming out of a "flex-builder -m ls1012ardb" just like the firmware above. No special settings yet, just following instructions and using a USB stick instead of an SD card yet, that's it.
What I am doing now is I completely cleaned my builds (inlc. rfs) and redo it clean way then reflash and I'll see.
I've you've other elements please share so I don't loose more time on looking for solution (even if I like doing that :smileywink:).
Thx Christophe