I have been analyzing the Errata for the LS1021A processor, LS1021ACE, Rev. 10, 11/2018. Specifically, I am looking at the workaround for A-010840. The workaround mentions a register bit DMR[SO]. I have looked in the reference manual, LS1021ARM Rev. 3 10/2018, and there is no bit called SO associated with this register. I was looking in section 30.2.1.2.
Is this a typo? Am I misreading this?
I will provide response through the dedicated Technical Case.
I am sorry. I posted this question minutes before I receive an answer from NXP support. I posted the question to NXP support on Feb 5th and didn’t receive an answer. I thought I would try the community site. Please disregard the question. Thank you
The bit is shown as reserved in the RM.
The DMR[SO] is bit 3.