FRWY LS1012A Download goes to 0B/s after 1.12GB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRWY LS1012A Download goes to 0B/s after 1.12GB

587 次查看
cdubs14
Contributor II

Hi,

 

I'm trying to execute the following sequence of commands to get the 5.10.35 Kernel Headers:

$ flex-builder -c linux-deb -p LS

Please copy linux-headers-5.10.35-dirty_5.10.35-dirty-4_arm64.deb to the target board and execute the following command.

# dpkg -i linux-headers-5.10.35-dirty_5.10.35-dirty-4_arm64.deb

# cd /usr/src/linux-headers-5.10.35-dirty

 

When downloading build files the download speeds always slows to zero sometime after the 1GB mark. This does not happen on my other Linux machine, so I'm suspecting it's the FRWY-LS1012A. Anyone else have this problem? See attached for photos

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

545 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Support of LS1012AFRWY with 1GB DDR, please boot up the target board from rootfs on SD card, then copy your files to SD card.

 

0 项奖励
回复

505 次查看
cdubs14
Contributor II

Hi @yipingwang ! I'm not sure how this solves the issue

0 项奖励
回复