ECC keys for Secure Boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECC keys for Secure Boot

Jump to solution
1,367 Views
nb1
Contributor I

Hi,

I'm trying to determine whether or not ECC keys are supported in ISBC, as Super Root Keys (SRKs).

The Trust Arch User Guide vaguely mentions "RSA or ECC private keys" for signing, but any other descriptions (including the LSDK User Guide), pictures or examples I've seen very specifically and exclusively refer to RSA keys up to 4K.

I'd appreciate if you could let me know whether ECC keys are supported, and if so, the supported curves please. If you could point me to some documentation that would be great as well.

Thank you!

0 Kudos
Reply
1 Solution
1,352 Views
bpe
NXP Employee
NXP Employee

ISBC supports only RSA. CST has no valid input file options for ECC in ISBC
headers. Only in the ESBC you have an option to use the ARM CoT for selecting
x509 format for ECC key or RSA key.

Best Regards,
Platon

 

 

View solution in original post

0 Kudos
Reply
2 Replies
1,353 Views
bpe
NXP Employee
NXP Employee

ISBC supports only RSA. CST has no valid input file options for ECC in ISBC
headers. Only in the ESBC you have an option to use the ARM CoT for selecting
x509 format for ECC key or RSA key.

Best Regards,
Platon

 

 

0 Kudos
Reply
1,344 Views
nb1
Contributor I

Thank you!

0 Kudos
Reply