Hi All ,
I am using SDK 1.7/1.8 for our custom board designed based on ls1021aiot. My question is Is there a support for Atheros wifi module. I have Module connected on mini PCIe and I can see foillowing when I do ''lspci -kv'
root@ls1021aiot:~# lspci -kv
0000:00:00.0 PCI bridge: Freescale Semiconductor Inc Device 0e08 (rev 20) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Memory at 4044000000 (32-bit, non-prefetchable) [size=16M]
Memory at 4040000000 (32-bit, non-prefetchable) [size=64M]
Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
[virtual] Expansion ROM at 4045000000 [disabled] [size=16M]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/16 Maskable- 64bit+
Capabilities: [70] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [148] #19
0001:00:00.0 PCI bridge: Freescale Semiconductor Inc Device 0e08 (rev 20) (prog-if 00 [Normal decode])
Flags: bus master, fast devsel, latency 0
Memory at 4844000000 (32-bit, non-prefetchable) [size=16M]
Memory at 4840000000 (32-bit, non-prefetchable) [size=64M]
Bus: primary=00, secondary=01, subordinate=01, sec-latency=0
Memory behind bridge: 46000000-460fffff
Prefetchable memory behind bridge: 46100000-461fffff
[virtual] Expansion ROM at 4845000000 [disabled] [size=16M]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/16 Maskable- 64bit+
Capabilities: [70] Express Root Port (Slot-), MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [148] #19
0001:01:00.0 Network controller: Qualcomm Atheros AR9580 Wireless Network Adapter (rev 01)
Subsystem: Qualcomm Atheros Device 3123
Flags: bus master, fast devsel, latency 0, IRQ 124
Memory at 4846000000 (64-bit, non-prefetchable) [size=128K]
[virtual] Expansion ROM at 4846100000 [disabled] [size=64K]
Capabilities: [40] Power Management version 3
Capabilities: [50] MSI: Enable- Count=1/4 Maskable+ 64bit+
Capabilities: [70] Express Endpoint, MSI 00
Capabilities: [100] Advanced Error Reporting
Capabilities: [140] Virtual Channel
Capabilities: [300] Device Serial Number 00-00-00-00-00-00-00-00
Is there a inbuilt driver support for "Qualcomm Atheros AR9580 Wireless Network Adapter" . Is there a module/driver that I need to enabled through menuconfig. Do I need to custom build the driver ? . Is there a basic support for atheros WIFI module.?? How can I enable it or use it?. Appreciate your help on this.
Thanks
Dhruval
NXP SDK for LS1021A-IOT board supports Atheros wifi module. See attached files. These files are screenshot from kernel menu from NXP SDK for LS1021A-IOT board.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Which SDK I can use for this ? I did tried to do menuconfig on my yocto for kernel but I did not find any thing for it. DO I need to purchase Atheros support ? Is there a special way to invoke/build this module ?