Can SGMI(2.5) be connected to 2500Base-x in ls1043a?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can SGMI(2.5) be connected to 2500Base-x in ls1043a?

ソリューションへジャンプ
561件の閲覧回数
lijun10210
Contributor III

The SGMII(2.5G) mode of ls1043 is connected to AQR115C 2500base-x.

My status is:PHY link is ok,but  the ping and PHY  loopback tests are fail。

I don't know why it's like this, is it because SGMII(2.5G) and 2500base-x are incompatible?

Hope for your answer,thanks a lot。

0 件の賞賛
返信
1 解決策
549件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @lijun10210,

Please refer to section# 33.2.1 mentioned in LS1043ARM in which the supported features are mentioned.

Regards,
Mrudang

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
550件の閲覧回数
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @lijun10210,

Please refer to section# 33.2.1 mentioned in LS1043ARM in which the supported features are mentioned.

Regards,
Mrudang

0 件の賞賛
返信