Can SGMI(2.5) be connected to 2500Base-x in ls1043a?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can SGMI(2.5) be connected to 2500Base-x in ls1043a?

Jump to solution
769 Views
lijun10210
Contributor III

The SGMII(2.5G) mode of ls1043 is connected to AQR115C 2500base-x.

My status is:PHY link is ok,but  the ping and PHY  loopback tests are fail。

I don't know why it's like this, is it because SGMII(2.5G) and 2500base-x are incompatible?

Hope for your answer,thanks a lot。

0 Kudos
Reply
1 Solution
757 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @lijun10210,

Please refer to section# 33.2.1 mentioned in LS1043ARM in which the supported features are mentioned.

Regards,
Mrudang

View solution in original post

0 Kudos
Reply
1 Reply
758 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @lijun10210,

Please refer to section# 33.2.1 mentioned in LS1043ARM in which the supported features are mentioned.

Regards,
Mrudang

0 Kudos
Reply