LPCXpresso IDE v4.3.0 now available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso IDE v4.3.0 now available

476 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Sep 20 01:38:39 MST 2012
We are please to announce the release of LPCXpresso IDE v4.3.0, which is now available for Windows, Linux and Mac OS X platforms.

The changes in this release include:

* Added support for LPC18/43 internal flash parts
* Added support for LPC407x/8x parts
* Changed Windows installer to prevent installation into a directory containing a space
* Fixed Mac OS X installer to correctly install on Case-Sensitive files systems
* Smaller footprint flash driver code/data
* Restore RAM contents used for target-resident flash driver code/data
* Added bit-band alias regions support
* Added support for non-contiguous internal flash banks
* Improved loadable flash driver diagnostics
* Fixed erroneous flash verify errors for loadable flash drivers
* Fix part IDs for LPC11U3x
* Fixed checksum utility for NXP LPC2000 parts
* Fixed license issue on some newer Linux distros
* LPCXpresso license fixes

To download, visit http://lpcxpresso.code-red-tech.com/LPCXpresso/

Regards,
CodeRedSupport
0 Kudos
Reply
0 Replies