No protocol specified invalid command name "bind" while executing "::unknown bind Text <Tab>" ("uplevel" body line 1) invoked from within "uplevel 1 $next $args" (procedure "::obj::Unknown" line 3) invoked from within "bind Text <Tab>" (procedure "::InstallJammer::InitializeGui" line 19) invoked from within "::InstallJammer::InitializeGui " (procedure "::InstallJammer::InitInstall" line 68) invoked from within "::InstallJammer::InitInstall" (file "/installkitvfs/main.tcl" line 38978) |
sudo apt-get install libgtk2.0-0:i386 libpangox-1.0-0:i386 libpangoxft-1.0-0:i386 libidn11:i386 libglu1-mesa:i386 libxtst6:i386 |
sudo apt-get install libgtk2.0-0:i386 libxtst6:i386 libpangox-1.0-0:i386 \ libpangoxft-1.0-0:i386 libidn11:i386 libglu1-mesa:i386 \ libncurses5:i386 libudev1:i386 libusb-1.0:i386 libusb-0.1:i386 \ gtk2-engines-murrine:i386 libnss3-1d:i386 |
cd /lib/i386-linux-gnu sudo ln -sf libudev.so.1 libudev.so.0 |
$ /usr/local/lpcxpresso_8.2.2_650/lpcxpresso/lpcxpresso
(LPCXpresso:30217): Gtk-WARNING **: 14:50:59.992: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:50:59.992: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.401: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.401: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.425: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.425: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.456: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.456: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:01.305: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:01.305: Negative content width -1 (allocation 1, extents 1x1) while allocating gadget (node trough, owner GtkProgressBar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:01.305: Negative content width -1 (allocation 1, extents 1x1) while allocating gadget (node trough, owner GtkProgressBar)
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0xf6f7f1aa, pid=30217, tid=4156991232
#
# JRE version: Java(TM) SE Runtime Environment (8.0_65-b17) (build 1.8.0_65-b17)
# Java VM: Java HotSpot(TM) Client VM (25.65-b01 mixed mode linux-x86 )
# Problematic frame:
# C [libX11.so.6+0x261aa] XDefaultRootWindow+0x1a
#
# Core dump written. Default location: /home/robin/Downloads/lcpxpresso/core or core.30217
#
# An error report file with more information is saved as:
# /home/robin/Downloads/lcpxpresso/hs_err_pid30217.log
#
# If you would like to submit a bug report, please visit:
# http://bugreport.java.com/bugreport/crash.jsp
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
Aborted (core dumped)
Got the install working using the --console mode option.
Windows come up blank but with lots of modal error windows titled "error" but with no text in them and an OK button.
Then it core dumps.
$ /usr/local/lpcxpresso_8.2.2_650/lpcxpresso/lpcxpresso
(LPCXpresso:30217): Gtk-WARNING **: 14:50:59.992: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:50:59.992: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.401: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.401: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.425: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.425: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.456: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:00.456: Negative content height -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:01.305: Negative content width -6 (allocation 1, extents 4x3) while allocating gadget (node toolbar, owner GtkToolbar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:01.305: Negative content width -1 (allocation 1, extents 1x1) while allocating gadget (node trough, owner GtkProgressBar)
(LPCXpresso:30217): Gtk-WARNING **: 14:51:01.305: Negative content width -1 (allocation 1, extents 1x1) while allocating gadget (node trough, owner GtkProgressBar)
#
# A fatal error has been detected by the Java Runtime Environment:
#
# SIGSEGV (0xb) at pc=0xf6f7f1aa, pid=30217, tid=4156991232
#
# JRE version: Java(TM) SE Runtime Environment (8.0_65-b17) (build 1.8.0_65-b17)
# Java VM: Java HotSpot(TM) Client VM (25.65-b01 mixed mode linux-x86 )
# Problematic frame:
# C [libX11.so.6+0x261aa] XDefaultRootWindow+0x1a
#
# Core dump written. Default location: /home/robin/Downloads/lcpxpresso/core or core.30217
#
# An error report file with more information is saved as:
# /home/robin/Downloads/lcpxpresso/hs_err_pid30217.log
#
# If you would like to submit a bug report, please visit:
# http://bugreport.java.com/bugreport/crash.jsp
# The crash happened outside the Java Virtual Machine in native code.
# See problematic frame for where to report the bug.
#
Aborted (core dumped)
SOLVED
I've got the same error invalid command name "bind" on Debian.
The problem, in my case, was /tmp partition that was not executable.
You can check your partitions typing the command mount and fix the problem with
mount -o remount,exec /tmp
Regards.
Paolo
sudo ./Installer_LPCXpresso_8.0.0_526_Linux-x86 --mode console |
The default install tries to use something called InstallJammer. This was a general purpose installer using tcl/tk that was supposed to look like the windows installer. According to wiki this has not been maintained since 2011.