Content originally posted in LPCWare by gusika on Sun Sep 21 17:38:48 MST 2014
Hello,
Freshly downloaded, installed and registered the lpcxpresso.
That's because the previous version could not be programmed correctly of the LPC1778 device. (4.1.0_190)
The previous version programmed correctly of the LPC1225!
After booting the first command line I typed:
"C:\nxp\LPCXpresso_7.3.0_186\lpcxpresso\bin\crt_emu_cm3_nxp -wire=hid -e0 -g -s100 -pLPC1778 -flash-mass"
LPCXpresso response:
-------------------------------------------------------------------------------------------------------------
Ni: LPCXpresso Debug Driver v7.3 (Jul 2 2014 14:55:57 - crt_emu_cm3_nxp build 10)
Pc: ( 0) Reading remote configuration
Pc: ( 5) Remote configuration complete
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Conn&Reset. DpID: 2BA01477. Info: HID64HS12
Nc: SWD Frequency: 100 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0 Poll delay: 0.
Nc: Loaded LPC177x_8x_407x_8x_512.cfx: LPC177x_8x_407x_8x (512K) Jul 1 2014 11:
51:12 On-chip Flash Memory
Nc: NXP: LPC1778 Part ID: 0x00000000
Pc: ( 65) Chip Setup Complete
Cr:v LPCXpresso Free License - Download limit is 256K
Pc: ( 70) License Check Complete
Nt: Mass Erase
Ec: Flash driver "EraseChip" return code: 0x1
Ed:04: Failed to erase flash: Ef(38). Flash operation has returned an error (see log).
Pc: (100) Target Connection Failed
-------------------------------------------------------------------------------------------------------------
???