LPCXpresso 1769 Reset behaviour

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso 1769 Reset behaviour

207件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by boater on Tue Jul 09 05:37:09 MST 2013
Hello

I have a weird issue with a LPCXpresso 1769 board, mounted on a protoboard. In case the 1769 is powered over the 3.3V pin only, it seems that LPCLink part gets powered as well, causing the Reset line to go low. Interestingly, power goes away e.g. when I put the cap on the JTAG pins and remove it, so perhaps something gets charged and is discharged by those kind of actions. Is the circuit so sensitive? Is there any advise on how to deal with this?

Thanks,
Peter
0 件の賞賛
返信
0 返答(返信)