For LPC18S37 should I be using the LPCXpresso IDE rather than the MCUXpresso?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

For LPC18S37 should I be using the LPCXpresso IDE rather than the MCUXpresso?

458 Views
GregT
Contributor III

The debugger terminates after a few minutes every time I try to attach.  When attached it seems to work.  I can pause and look thru memory.  If I need to use the LPCXpresso IDE please put in a link for the download.

Thanks!

0 Kudos
Reply
1 Reply

439 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @GregT,

Could you please share with us where it stopped? If an error window appears, could you share that too?

Are you using an NXP EVK or a custom board? Could you please try debugging an example from LPCOpen? Is the same behavior happening?

Could you please check you have selected the correct LPC18xx Internal Flash Driver? Please right click on Properties -> C/C++ Build -> MCU settings, then add a specific flash driver for the flash you want to program. You could also check more information regarding this in the MCUXpresso IDE User Guide.

Kind regards, Raul.

0 Kudos
Reply