EM773 Supported on LPCXpresso 4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EM773 Supported on LPCXpresso 4

972 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TGerrits on Wed Sep 07 01:28:12 MST 2011
Quoting an old thread from January 2011 asking for EM773 to be suported by LPCxpresso, Neal Frager said that:

"1. Right now, we are waiting on Code Red Xpresso version 4 which will be  EABI compliant. (...) ce version 4 is released from Code Red, you are welcome to try porting the SDK over to Xpresso. "

Well version 4 of LPCXpresso is already running, when are you planning to released a supported SDK of the EM773 on LPCXpresso4 IDE ?

BR,
T.G:
0 项奖励
回复
4 回复数

958 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bernhardfilzmaier@gmx.at on Sat Feb 16 08:57:51 MST 2013
ahh sorry and thanks :)
0 项奖励
回复

958 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Feb 16 08:37:53 MST 2013
What about EM773/301 or EM773/302 in LPC11xx folder ('Target selection' window) :confused:
0 项奖励
回复

958 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bernhardfilzmaier@gmx.at on Sat Feb 16 03:56:21 MST 2013
Hi i cannot find the EM773 in de MCU list, i am using LPCXpresso  v5.1.0... if i open the projekt of the SDK2.1 the selected target in the  MCU settings is LPC1114/302?
0 项奖励
回复

958 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pat on Sat Jul 14 14:14:57 MST 2012
A bit late though I noticed that the EM773 SDK2.0 release has LPCXpresso support...
0 项奖励
回复