I have a PNEV512B with a LPCXpresso LPC1769development board which I'm using to try out the PN512 device. I've been following the AN11308 guide on this. I've now got LPCXpresso building code ready for release. Prior to this I had to follow the .dll Cygwin issue fix here. The code I'm building is SW2979.
The issue is that Redlink cannot see my device. In Device Manger it comes up as a comport only and does not come up as a "USB Device with DFU Capabilities". I've tried updating drivers from all over the NXP site but haven't passed this point.
This is the error I'm getting in LPCXpresso:
[Started server]
[Connected on port 3025]
redlink>ProbeList
No probes found
redlink>ProbeList
No probes found
redlink>ProbeStatus
redlink>quit
[Closed]
I've also tried using MCUXpresso but am getting build issues of files missing.
I've spent more than a day working on this when I thought that because I had the OTS hardware I'd be up and running in no time.
Hello sir,
Sorry for asking once again but, could you please clarify that you have already installed the SDK available in the PN512 site? The file name is: AN10664_1_NFC_FRI_SDK_206810
In case you followed the instructions of the Application note and, the issue is still persistent, please let me know.
Some screen shots and an output log will be greatly appreciated.
Hello, my name is Fabian, I've been assigned to support your case.
Thank you for your interest in our products
First I have to mention that we don't fully recommend PN512 IC for new designs. We do have a version for the NFC Reader Library available in the following link: https://www.nxp.com/design/design-center/development-boards-and-designs/nfc-reader-library-software-...
Please go to Downloads section and, click on the Download Button.
Keep in mind that the latest update for PN512 is from 2016 but, it is built for working with the LPC1769 board.
Still, please explore the possibility of using one of our latest ICs: https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers:NFC-READER
HI Fabian,
Good to know on the NRND of the PN512. It's a shame to hear because the PN512 doesn't say this and neither does any of the documentation. I have therefore wasted about 2.5 days of work in this case.
Do you have any suggestions regarding the error I've raised in the support ticket please? I'm yet to get support to fix the issue I posted. I've got the PNEV512 and LPC1769 hardware, the LPCXpresso v8.2.2_650 IDE, the SW2979 firmware and I'm following the AN11308. See error in ticket.
Thanks, Louis
Hello louis____
This AN uses demo with LPCXprsso IDE. Thus to avoid confusing, I would suggest you working on the same enviroment. Here is LPCXpresso IDE download. please try and see how it works.
Best Regards,
Jun Zhang
Hello sir,
At this point it is difficult to determine what could cause the issue with the connection. Please take a look at the PN512 site: https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/standard-nfc-frontend:PN512
In the Documentation section, please expand it and, locate: AN10664_1_NFC_FRI_SDK_206810
This is an executable and, has an application note, it may fix the driver issue.