Hi,
I try to implement a Vcom Port (CDC) on an PN7462. I need to use USBD_ROMStack.
But this folder is greyed out and strike through. I searched a lot, but wasn't able to find the meanig
of the grey folders and files.
Im sure this is no big issue.
Best Regards
Mario
解決済! 解決策の投稿を見る。
Are these folder perhaps marked as excluded from the build? Right click on them in the Project Explorer view and check the settings in the "Resouce Configurations" entry.
I also note that your project is using linked references. Make sure these folders actually exist in the linked location.
Regards,
LPCXpresso Support
Hi,
thank you for your reply. No this files are not excluded from the build. The folders are
also existing. It's from the PN7462 examples witch you can download from here:
Best Regards
Mario
Hi Con Verse,
thank you very much. This solved my problem.
Best Regards
Mario