PCF8563
Now we just check and compare with a PCF8563 data sheet and real register value.
but our real 01h value and a data sheet value is different
our register value
01h - 0x80 , 0xC0
on data sheet
01h - N (0x00)
we compare with a TABLE 4. Formatted registers overview
can you check that problem please?
已解决! 转到解答。
Thank you for replying
other reset register value is same all right but 01h reset register value is different with a data sheet
Table 27. Register reset value[1]
01h Control_status_2 0 0 0 0 0 0 0 0
thank you for replying
reset value 01h real value and 01h data sheet value is different does it make any problem? or error?
PCF8563 Reset value
00h | 01h | 02h | 03h | 04h | 05h | 06h | 07h | 08h | ||
LOT | XD842 | 0x08 | 0x00 | 0x80 | 0x00 | 0x00 | 0x01 | 0x00 | 0x01 | 0x00 |
XD920 | 0x08 | 0x00 | 0x80 | 0x00 | 0x00 | 0x01 | 0x00 | 0x01 | 0x00 | |
XD915 | 0x08 | 0x80 | 0x90 | 0xF4 | 0xA2 | 0xAD | 0x94 | 0x1C | 0x85 | |
nG936 | 0x08 | 0xC0 | 0xD7 | 0xBF | 0xEC | 0xFA | 0xD3 | 0x59 | 0xB9 | |
nG038 | 0x08 | 0xC0 | 0xE8 | 0x83 | 0xF8 | 0xC7 | 0xEF | 0x76 | 0x71 |
Thank you for replying
other reset register value is same as data sheet ,but 01h reset register value is different with a data sheet
Table 27. Register reset value[1]
01h Control_status_2 0 0 0 0 0 0 0 0