nxpUSBlib CDC class

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

nxpUSBlib CDC class

1,509件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mshrestha789 on Thu May 22 02:06:53 MST 2014
Hello friends,

In errata sheet it is return "The CDC class USB ROM drivers return a STALL condition after the DATA stage of a Set Line Coding CONTROL transfer from the host". Is this still a problem in the provided driver or is it already fixed? Any help regarding this will be highly appreciated.
ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,491件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri May 23 12:55:05 MST 2014
Hi

The bug exists only in Revision A parts as stated in the errata sheet. This has been fixed in Rev C parts.

Thanks
NXP Technical Support
0 件の賞賛
返信