Hi
Want to know the behavior HSADC_DESC_MATCH(0x0) and HSADC_DESC_THRESH_A below example,
As my undestand,
In this case. which behavior will be higher priority? simpling imediataly or wait unitl THRSH_A trigger?
Chip_HSADC_SetupDescEntry(LPC_ADCHS, 0, 0, (HSADC_DESC_CH(1) |
HSADC_DESC_BRANCH_NEXT | HSADC_DESC_MATCH(0x1) | HSADC_DESC_THRESH_A |
HSADC_DESC_RESET_TIMER));
已解决! 转到解答。
Hi,
I suppose that you misunderstood the threshold_A, it is not a trigger source, it is a compare register, the ADC sample result is compared with the threshold_A register automatically, then update flag or fire interrupt which indicates that the analog signal is below a threshold or above a threshold.
If you set HSADC_DESC_MATCH(0x10), the adchs module has an internal counter, the tick is the ADC clock, after hardware/software trigger, when the counter reaches 16 or 0x10, the ADC will convert, so the ADC conversion rate is Fadc/16.is you set HSADC_DESC_MATCH(0x00), the ADC will generate a sample for each ADC clock cycle.
Hope it can help you
BR
Xiangjun Rong
Hi,
Q1)HSADC_DESC_MATCH(0x0)will start sampling immediately in this case.
>>>>>The HSADC_DESC_MATCH(0x0) does not mean that the ADC converter starts-up immediately, the HSADC_DESC_MATCH(0xxx) can control the ADC sampling time(ADC conversion rate). Setting HSADC_DESC_MATCH(0x00) means that the ADC can get one sample for each ADC clock.
You can use software trigger to start ADC conversion by setting the SW_TRIGGER bit in Trigger register, pls refer to section 48.6.5 Trigger register.
You can use hardware trigger to start ADC conversion by setting the ADCHS_TRIGGER_IN reg, pls refer to section 18.4.25 ADCHS trigger input multiplexer (ADCHS_TRIGGER_IN).
Q2)and HSADC_DESC_THRESH_A will start simpling at trigger threshold_A.
>>>>>DESCRIPTOR0x[THRESHOLD_SEL] selects the ADC result comparsion threshold register, it is NOT related to ADC starting.
Hope it can help you
BR
XiangJun Rong
I don't quite understand.
Here a case of both HSADC_DESC_THRESH_A and HSADC_DESC_MATCH(0x10) set to descriptor.
then while threshold_A was trigger at hsadc timer 0x5, what is the timing clock of simpling? clock 0x5, 0x6 or 0x10?
thanks
Peter
Hi,
I suppose that you misunderstood the threshold_A, it is not a trigger source, it is a compare register, the ADC sample result is compared with the threshold_A register automatically, then update flag or fire interrupt which indicates that the analog signal is below a threshold or above a threshold.
If you set HSADC_DESC_MATCH(0x10), the adchs module has an internal counter, the tick is the ADC clock, after hardware/software trigger, when the counter reaches 16 or 0x10, the ADC will convert, so the ADC conversion rate is Fadc/16.is you set HSADC_DESC_MATCH(0x00), the ADC will generate a sample for each ADC clock cycle.
Hope it can help you
BR
Xiangjun Rong