LPC4337 and SSD1963

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4337 and SSD1963

1,066 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Bladerunner_Mike on Sun Jan 26 19:56:02 MST 2014
We've attached SSD1963 based tft dsyplay to EMC (signals: D15..D0 , RD#, WR#, CS#, A2). Dysplay require 8080-like bus for communication. In the 8080-mode interface consist of CS#, D/C#, RD#, WR#, D[16(8,9,24):0]  This interface use WR# to define a write cycle and RD# for read cycle. If the WR# goes low when the CS# signal is low, the data or command will be latched into the
system at the rising edge of WR#. Similarly, the read cycle will start when RD# goes low and end at the
rising edge of RD#. But interval between edges of WR# and CS# is too small, these signals are quite synchronous.

How to increase this interval?


The code of static init is following:

void emcStaticInit ()
{
        
        EMC_STATICWAITWEN0_bit.WAITWEN        = 0xF; //
        EMC_STATICWAITWR0_bit.WAITWR          = 0x1F;
        EMC_STATICWAITOEN0_bit.WAITOEN        = 0xF;
        EMC_STATICWAITPAGE0_bit.WAITPAGE      = 0xf;
        EMC_STATICWAITTURN0_bit.WAITTURN         = 0x1f;
                
       
        EMC_STATICWAITRD0_bit.WAITRD           = 0x1f;
        
        EMC_STATICCONFIG0_bit.B  = 0x0;
        
        EMC_STATICCONFIG0_bit.MW = 0x1;
        EMC_STATICCONFIG0_bit.PM = 0x0;
        EMC_STATICCONFIG0_bit.PB = 0x1;
        

}


In previous project we used GPIO for emulation 8080 bus interface, and initialization code of SSD1963 work well, and we could control diagrams of CS# WR# and D, A.

Labels (1)
0 Kudos
Reply
2 Replies

984 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Bladerunner_Mike on Mon Jan 27 19:22:25 MST 2014
Everything is OK! Very
0 Kudos
Reply

984 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Mon Jan 27 10:28:01 MST 2014
you need to insert NOPs in between the lines of code.
depending upon compiler, some thing like
asm volatile ("mov r0,r0");

will add one clock

EMC_STATICWAITWEN0_bit.WAITWEN        = 0xF; //
asm volatile ("mov r0,r0");
asm volatile ("mov r0,r0");
asm volatile ("mov r0,r0");
asm volatile ("mov r0,r0");
EMC_STATICWAITWR0_bit.WAITWR          = 0x1F;

will add 4 clocks
0 Kudos
Reply