LPC1343 USB to DALI Master demo board - DALI BUS Power Supply

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1343 USB to DALI Master demo board - DALI BUS Power Supply

1,755 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SteveJG on Sat Nov 28 09:48:36 MST 2015
Hi, to connect the LPC1343 USB to DALI Master demo board to the OM13026 LPC111x DALI slave demo board or a DALI luminaire driver/ballast do I need to connect a Helvar 401 or Tridonic PS1 or equivalent DALI bus power supply or is there another DALI BUS power supply option I can use? Thanks, Steve
标签 (1)
0 项奖励
回复
1 回复

1,456 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SteveJG on Sun Nov 29 14:38:26 MST 2015
Problem solved, I've noticed in the DALI Application note you can use a general lab power supply set at 16V output with 100ohm resistor and current set to 200mA Max. Cheers, Steve
0 项奖励
回复