LPC1317 peripheral on almost any pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1317 peripheral on almost any pins

ソリューションへジャンプ
3,065件の閲覧回数
MJ1
Contributor I

Hi

Is possible to reconnect/repin peripherals on LPC1317 HVQFN33 package to pins which are not intended in manual for that peripheral? I.e. UART/USART RXD, TDX signals to SPI MOSI, MISO - PIO0_21, PIO0_22 pins?

 

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
3,056件の閲覧回数
frank_m
Senior Contributor III

No.

Just like with the power supply and clock oscillator pins, the peripheral switch matrix options per pin are defined by the silicon. The possible configuration options per pin are given in the datasheet.

Alternatively, you could use a larger package, or implement some functionality by "bit-banging" (like a "software UART").

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,057件の閲覧回数
frank_m
Senior Contributor III

No.

Just like with the power supply and clock oscillator pins, the peripheral switch matrix options per pin are defined by the silicon. The possible configuration options per pin are given in the datasheet.

Alternatively, you could use a larger package, or implement some functionality by "bit-banging" (like a "software UART").

0 件の賞賛
返信
3,054件の閲覧回数
MJ1
Contributor I

Thanks so much.

0 件の賞賛
返信