Asier,
iap demo code isn't included in the older SDK package. But I just checked it was included in the latest SDK2.7. please download the latest SDK 2.7.0 then find it here:
\SDK_2.7.0_LPCXpresso802\boards\lpcxpresso802\driver_examples\iap
Have a great day,
Jun Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
the SDK of LPC80x series product haven't includes FALSH driver.
In fact, the LPC802 flash driver use IAP command, so you can refer to the Code Bundle code:
LPC802 Example Code Bundle MCUXpresso
Also there is a Application about using EEPROM on LPC802, you can refer to the code and how to
using IAP command to erase, write flash, etc.
https://www.nxp.com/docs/en/application-note/AN12125_LPC802.zip
or
LPC804 SPI Secondary Bootloader
Have a great day,
Jun Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
SDK for LPC802 includes "IAP Driver version 2.0.2" option to include when doing "New project...".
I'm using SDK_2.x_LPC802 and version 2.6.0 (228 2019-06-14).
I'm searching an example of using following functions includes at fsl_iap.c driver:
status_t IAP_PrepareSectorForWrite(uint32_t startSector, uint32_t endSector);
status_t IAP_CopyRamToFlash(uint32_t dstAddr, uint32_t *srcAddr, uint32_t numOfBytes, uint32_t systemCoreClock);
....
Best regards,
Asier.
Asier,
iap demo code isn't included in the older SDK package. But I just checked it was included in the latest SDK2.7. please download the latest SDK 2.7.0 then find it here:
\SDK_2.7.0_LPCXpresso802\boards\lpcxpresso802\driver_examples\iap
Have a great day,
Jun Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------