I have procured 25 numbers of LPC1788FBD208 on which the following markings are there:
LPC1788FBD208
SKP483.1
ZSD1821E
Hello jayanthy M.S. ,
Thanks for contacting our technical support, I will serve for you.
From the marking of your chip, the year of the device was manufactured is the Week 21 of 2018.
It seems this data sheet lost the Marking part, so please have a look at the Errata sheet, in Part I Product identification:
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Alice_Yang,
Thanks for the information.
With Best Regards,
Jayanthy M.S.
On Mon, 18 Feb 2019 04:23:00 +0000 (UTC), Alice_Yang wrote
NXP Community
Re: How to identify the Date code/year of manufacture of LPC1788FBD208
reply from Alice_Yang in LPC Microcontrollers - View the full discussion