How to enable function SGPIO to meet SFF-8485 Specification SFF-8485 REV0.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to enable function SGPIO to meet SFF-8485 Specification SFF-8485 REV0.7

ソリューションへジャンプ
3,463件の閲覧回数
carter_wang
Contributor I

 

Hi,

 

We use chip LPC5526JBD64E to get the status of hard drives from the host via SGPIO.

I was wondering whether the chip supports the SGPIO function?
If the answer is yes, how to enable it?

 

BR,

carter

0 件の賞賛
返信
1 解決策
3,418件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cater

Here are some  application notes on how to use SGPIO on LPC4300. If source codes exist, they are included in the zip files:

SGPIO on the LPC4300:
https://www.nxp.com/docs/en/application-note/AN11275.zip

Using SGPIO to emulate an SPI master interface:
https://www.nxp.com/docs/en/application-note/AN11210.zip

LPC4300 camera interface design using SGPIO:
https://www.nxp.com/docs/en/application-note/AN11196.zip

SGPIO camera module design using LPC4300:
https://www.nxp.com/docs/en/application-note/AN11343.zip

Implementing a UART using SGPIO on LPC4300:
https://www.nxp.com/docs/en/application-note/AN11351.zip

 

Hope this helps.

Jun Zhang

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,446件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Carter

Please read this application note. this is 

https://www.nxp.com.cn/docs/en/application-note/AN12326.pdf

but we don't have qualification of SFF-8485 Specification. 

Have a nice day,

Jun Zhang

0 件の賞賛
返信
3,442件の閲覧回数
carter_wang
Contributor I

 

Hi Jun,

 

Thanks for your information.

However, I am looking forward to Serial General Purpose Input Output(SGPIO), not secure gpio.

 

BR,

carter

0 件の賞賛
返信
3,434件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cater.

No. LPC55 doesn't support Serial General Purpose Input Output(SGPIO).

our LPC43xx supports Serial GPIO, but LPC55 doesn't.

Hope this helps,

Jun Zhang

0 件の賞賛
返信
3,429件の閲覧回数
carter_wang
Contributor I

 

Hi Jun,

 

Got it.

I was wondering if you could share the source code of SGPIO with us?

 

BR,

carter

0 件の賞賛
返信
3,419件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cater

Here are some  application notes on how to use SGPIO on LPC4300. If source codes exist, they are included in the zip files:

SGPIO on the LPC4300:
https://www.nxp.com/docs/en/application-note/AN11275.zip

Using SGPIO to emulate an SPI master interface:
https://www.nxp.com/docs/en/application-note/AN11210.zip

LPC4300 camera interface design using SGPIO:
https://www.nxp.com/docs/en/application-note/AN11196.zip

SGPIO camera module design using LPC4300:
https://www.nxp.com/docs/en/application-note/AN11343.zip

Implementing a UART using SGPIO on LPC4300:
https://www.nxp.com/docs/en/application-note/AN11351.zip

 

Hope this helps.

Jun Zhang

0 件の賞賛
返信
3,298件の閲覧回数
carter_wang
Contributor I

 

Hi Jun,

 

I tried to simulate SGPIO slave device via sensing gpio signals by software.

However, it seems impossible.

Am I right?

 

BR,

carter

0 件の賞賛
返信
3,399件の閲覧回数
carter_wang
Contributor I

 

Hi Jun,

 

Thanks for your information.

Have a good day~

 

BR,

carter

0 件の賞賛
返信