Can LPC2478FET208,551 replace a LPC2470FET208,551 design?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can LPC2478FET208,551 replace a LPC2470FET208,551 design?

713 次查看
jetbig
Contributor I

The LPC2470 has no flash.  Wanted to know if the LPC2478 can drop in replace the LPC2470 and not use its on board flash?  Is there something special we need to do with the LPC2478 to get it to not use its onboard flash?

0 项奖励
回复
3 回复数

701 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

LPC2470 is flashless version of LPC2478. they are pin to pin replacement.

theoretically, you use LPC2470 project directly on LPC2478. 

0 项奖励
回复

697 次查看
jetbig
Contributor I

So are you saying that an unprogrammed LPC2478 will automatically act like a flashless LPC2470 and directly load the external program without any special configuration?

0 项奖励
回复

692 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

yes, just make sure your LPC2478 board has the same PCB design as LPC2470.

LPC2470 project can work on LPC2478 directly.

 

0 项奖励
回复