Hello an jian,
I just was wondering which board ?
For example LPCXpresso board for LPC1769, you can download schematic on NXP website:
LPCXpresso board for LPC1769 with CMSIS DAP probe|NXP
Hope it helps,
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
您好:
是这样的,我要用Altium Designer软件画工程电路设计图。我需要贵公司支持的芯片图,与封装文件,我记得以前在公司的网站上可以下载的,为什么现在下载不到呢。这样我就不用自己画芯片的原理图引脚了
发送自 Windows 10 版邮件<https://go.microsoft.com/fwlink/?LinkId=550986>应用
I need to use atium designer to design the circuit diagram and lpc1769 chip. Now I need the schematic diagram and pin diagram of the chip and the PCB package engineering library file.I don't know if you can understand me
Hello an jian,
There is only the LIB for ORCAD, no Altium Designer.
LPC1769FBD100|Arm Cortex-M3|32-bit MCU|NXP
Maybe you can try to search , whether there is a method to convert it to Altium Designer Lib.
BR
Alice