Does emWin include a simulator which graphic designer can design without evaluation board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does emWin include a simulator which graphic designer can design without evaluation board?

1,832件の閲覧回数
lpcware-support
Senior Contributor I

The PC simulation of emWin allows you to compile the same "C" source on your Windows PC using a native (typically Microsoft) compiler and create an executable for your own application. The resulting executable can be easily sent via email. With the simulator, you can design the user interface on your PC (no need for hardware!), debug your user interface program, and create demos of your application, which can be used to discuss the user interface.

ラベル(2)
タグ(2)
0 件の賞賛
返信
0 返答(返信)