When you need to create copy/clone of i.g. web_hvac example for FreeRTOS as standalone project, you can face this issue.
It is impossible to work with the copy.
Why? There is missing folder for RTOS and LIB.
ISSUE:
You start to clone example
There is missing folder for RTOS
Also missing library ksdk_freertos_lib which is needed for the example
Impossible to compile the project, because folder mentioned above are missing in the project
WORKAROUND:
Just add the folder rtos from C:\Freescale\KSDK_1.3.0
The same for the library, you add to the folder from C:\Freescale\KSDK_1.3.0\lib
Import .wsd file
Wsd file was successfully imported, library is included
Build successful finished
I hope this helps you.
Iva
Iva,
Has this been corrected in the 2.0 version of the KSDK Project Generator?
Allen
Hello Allen,
unfortunately not.
The issue occurs when you generate project as standalone project.
When you generate project to user_apps folder, there is no issue and it works without problem.
Have a nice day.
-Iva