startup sequence in detail of kinetis microcontrollers

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

startup sequence in detail of kinetis microcontrollers

1,659 次查看
josephxavier
Contributor III

can anyone share me a link to study the  startup sequence in detail of kinetis microcontroller. I need to prepare a presentation on it.

标签 (1)
0 项奖励
回复
1 回复

1,353 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi josephxavier,

   About the startup sequence, if you find a kinetis sample code, it doesn't difficult to understand.

   1. POR and the chip is reset

   2. enter in the Reset_Handler, which you can find it from the .s file.

take KL25 KSDK1.3.0 sample code as an example.

Reset_Handler

        CPSID   I               ; Mask interrupts

        LDR     R0, =SystemInit

        BLX     R0

        LDR     R0, =init_data_bss

        BLX     R0

        CPSIE   I               ; Unmask interrupts

        LDR     R0, =__iar_program_start

        BX      R0

        PUBWEAK NMI_Handler

        SECTION .text:CODE:REORDER:NOROOT(1)

3. enter the SystemInit function.

this function will have the disable watchdog code and the clock setup code, for details, please refer to the sample code.

4. enter init_data_bss function

  this function is make necessary initializations for the RAM

5. enter main function, which you can find it from __iar_program_start

Besids, in the K series and KL series  quick reference, there still have some startup routines description, you can refer to it.

http://cache.nxp.com/files/32bit/doc/quick_ref_guide/KQRUG.pdf?fpsp=1&WT_TYPE=Quick%20Reference%20Gu...

chapter 1.1.4.2 Startup routines

Wish it helps you!

If you still have question, please contact with me!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复