HI,
In my application I need to switch periodically between run mode and very low power stop mode. I use the RTC alarm interrupt to exit the stop mode which works just fine. However, after exiting the stop mode the serial communication stops working. Do I need to deinit the uart before entering the stop mode and initializes it again after exiting? hope someone can help me? thanks
Hi
It is not necessary to re-initialie anything at the UART after exiting VLPS.
See the following https://community.freescale.com/message/421247#421247
Regards
Mark
Hi Mark,
Thank you for your reply, linker should be:
https://community.nxp.com/message/421247#421247
Otherwise, it will be the wrong link.
Best Regards,
Kerry