eGUI 3.0.0: TWR_K60N512 "Audio" Demo for KDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

eGUI 3.0.0: TWR_K60N512 "Audio" Demo for KDS

eGUI 3.0.0: TWR_K60N512 "Audio" Demo for KDS

This is a port of the TWR_K60N512 "Audio" Demo into Kinetis Design Studio and into eGUI 3.0 (from 2.1).

The original demo is from Gargy and was under "Freescale_embedded_GUI_SW.zip\_Official_Demos\EGUI_D4D_Demo\TWR_K60N512\BareMetal\CW_10_1" avaiable on the freescale website.

Some of the major porting differnces (this may help others porting similar projects):

KDS:

eGUI 2.1 -> 3.0:

  • Autosize feature has gone, all object sizes now need to be declared
  • Objects seem to add padding of some sort: even with objects where size was previously declared, these had to be increased by ~3px in each direction, else text/images would not render.
  • 'D4D_OBJECT_SYS_FUNCTION' structure no longer contains 'type'. It suggests using strName instead to identifier object.
  • D4D_TEXTBOX no longer has title or icon functionality.

When building this project there will be ~7 warnings from the compiler, including 2 of my own. The code should function fine.

note: TWR_LCD settings for this project, switches are set up with in following sequence: "01111110".

regards,

Rael S-R

附件
无评分
版本历史
最后更新:
‎07-08-2014 06:32 AM
更新人: