I'm trying to find the major differences between the TWR-K21F120M and TWR-K21F120MA which lead to the micro-controlers, MK21FN1M0AVMC12 and the MK21FN1M0VMC12. So What is the difference between the MK21FN1M0AVMC12 and the MK21FN1M0VMC12; is it just the analog modules and the extra memory type?
解決済! 解決策の投稿を見る。
Hi Brent,
Actually, there are same except for the different Silicon Rev.
The A means the Production Rev A and the Fig 1 illustrates the more information about it.
Fig 1
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Brent,
Actually, there are same except for the different Silicon Rev.
The A means the Production Rev A and the Fig 1 illustrates the more information about it.
Fig 1
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Yes, that is the question. If it is just a few extra features like analog stuff then I might get the cheaper of the two.
In the datasheet:
http://cache.nxp.com/files/32bit/doc/data_sheet/K21P121M120SF5V2.pdf
in section '3.8.10.4 Part identification' it gives you a break down of the part numbers for the differences. Looks like 'A' denotes silicon Rev 'Revision after main'. Quite what that means I'm not sure. Or is that the question?
Yes, that is the question. If it is just a few extra features like analog stuff then I might get the cheaper of the two.