this is the Kinetis KEA64 datasheet (Document number: S9KEA64Z64M20SF0RM). On this page there is clearly a compilation error: does anyone have one or more more up-to-date revision? Thank you
已解决! 转到解答。
Hi Fabrizio Ferrari,
Thank you very much for your question, and tell us the doc bug.
After check the KEAZN64 header file SKEAZN642.Hl
/* FPROT Bit Fields */
#define FTMRH_FPROT_FPLS_MASK 0x3u
#define FTMRH_FPROT_FPLS_SHIFT 0
#define FTMRH_FPROT_FPLS(x) (((uint8_t)(((uint8_t)(x))<<FTMRH_FPROT_FPLS_SHIFT))&FTMRH_FPROT_FPLS_MASK)
#define FTMRH_FPROT_FPLDIS_MASK 0x4u
#define FTMRH_FPROT_FPLDIS_SHIFT 2
#define FTMRH_FPROT_FPHS_MASK 0x18u
#define FTMRH_FPROT_FPHS_SHIFT 3
#define FTMRH_FPROT_FPHS(x) (((uint8_t)(((uint8_t)(x))<<FTMRH_FPROT_FPHS_SHIFT))&FTMRH_FPROT_FPHS_MASK)
#define FTMRH_FPROT_FPHDIS_MASK 0x20u
#define FTMRH_FPROT_FPHDIS_SHIFT 5
#define FTMRH_FPROT_RNV6_MASK 0x40u
#define FTMRH_FPROT_RNV6_SHIFT 6
#define FTMRH_FPROT_FPOPEN_MASK 0x80u
#define FTMRH_FPROT_FPOPEN_SHIFT 7
SO, the FPROT register should be the same as the KEA128:
About the KEA64 reference manual problem, I will report it to our according department, it will be updated in the next RM version.
Thank you again.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Through various documents found I was able to understand that it was similar to that of KEA128 and to be able to proceed with the project in the meantime, but I thank you very much for this post of confirmation. Greetings and thanks again
Fabrizio.
Hi Fabrizio Ferrari,
Thank you very much for your question, and tell us the doc bug.
After check the KEAZN64 header file SKEAZN642.Hl
/* FPROT Bit Fields */
#define FTMRH_FPROT_FPLS_MASK 0x3u
#define FTMRH_FPROT_FPLS_SHIFT 0
#define FTMRH_FPROT_FPLS(x) (((uint8_t)(((uint8_t)(x))<<FTMRH_FPROT_FPLS_SHIFT))&FTMRH_FPROT_FPLS_MASK)
#define FTMRH_FPROT_FPLDIS_MASK 0x4u
#define FTMRH_FPROT_FPLDIS_SHIFT 2
#define FTMRH_FPROT_FPHS_MASK 0x18u
#define FTMRH_FPROT_FPHS_SHIFT 3
#define FTMRH_FPROT_FPHS(x) (((uint8_t)(((uint8_t)(x))<<FTMRH_FPROT_FPHS_SHIFT))&FTMRH_FPROT_FPHS_MASK)
#define FTMRH_FPROT_FPHDIS_MASK 0x20u
#define FTMRH_FPROT_FPHDIS_SHIFT 5
#define FTMRH_FPROT_RNV6_MASK 0x40u
#define FTMRH_FPROT_RNV6_SHIFT 6
#define FTMRH_FPROT_FPOPEN_MASK 0x80u
#define FTMRH_FPROT_FPOPEN_SHIFT 7
SO, the FPROT register should be the same as the KEA128:
About the KEA64 reference manual problem, I will report it to our according department, it will be updated in the next RM version.
Thank you again.
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------