UART terminal output scrambled using KL26Z64 and FT232RL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

UART terminal output scrambled using KL26Z64 and FT232RL

1,715 次查看
gustavsl
Contributor III

Hi. I am using KL26Z64 on a custom board without an external crystal, running at 41.94304MHz.

I'm using USBDM on a FRDM-KL25Z for programming and debugging.

I'm using UART (at 1310720 baud) to achieve serial communication using a FT232RL serial-to-USB converter.

I'm acquiring samples from a microphone using the ADC configured to 8-bit.

I'm converting the samples to output ASCII to a terminal.

The issue is that my data is randomly corrupted. For example, when the ADC reads a value of 94 or 95, it shows up on the Terminal as follows:

094

095

094

094

094

095

095

095

094

095

094

...

But randomly data shows up scrambled:

094

095

094

0

950094

095

095

094

...

I checked the clock settings and the timing for any interrupt starvation but that's not the case.

The code is as follows:

for(;;)

  {   

       LED1_On(); //LED on for time measuring

       AD1_Measure(TRUE);

       AD1_GetValue8(&leitura);

       // Converting to ASCII

       while (leitura >= 0 && i < 3)

       {  

            caractere = leitura % 10;

            charEnviar[i] = (caractere | mask);

            leitura = leitura / 10;

            i++;

       }

       // Send to terminal

       AS1_SendChar(charEnviar[2]);

       AS1_SendChar(charEnviar[1]);

       AS1_SendChar(charEnviar[0]);

       AS1_SendChar('\n');

       i = 0;

       LED1_Off();

  }


Thanks,

Gustavo.

标签 (1)
标记 (4)
0 项奖励
回复
1 回复

1,469 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Gustavo

probably the problem is the serial-to-USB converter. Have you check with the oscilloscope, if the signal from the Serial (kl26) is correct?

What happened if you only send data through the serial port? like only "test", did you see the same problem?

Regards

Vicente

0 项奖励
回复