Hi,
I was just trying to use the TWR-K53N512 with MED-EKG. But as given in UserGuide, I donot have a TWR-SER. Can I use a TWR-K70F120M instead for connectivity? Can I also get pointers on building this tower system?
Many Thanks,
Soumya
Hi Soumya KS,
Please give me what the userguide you are reading.
You can't use the TWR-K70F120M board instead of TWR-SER. But you can check it, what the detail function used with TWR-SER, you can find other hardware to replace. Take an example, if it is just use the UART, you can find a TTL to USB tool to replace the TWR-SER.
But to work easily, it's better to work with TWR-SER:
Serial (USB, Ethernet, CAN, RS232/485) Tower System Module|NXP
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------