SAI I2S blocking kl17, EDMA vs DMA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SAI I2S blocking kl17, EDMA vs DMA

2,046 次查看
jacobjennings
Contributor III

Hello,

 

I have a few questions surrounding the attached simple example project transmitting I2S data against an MKL17Z256VFM4. First, is it possible to transmit continuously without delay using a circular ping pong DMA buffer without using 2 DMA channels? Does that require EDMA (not on MKL17)? Why doesn't the __asm("bkpt #0") breakpoint in main ever trigger (why does SAI_DRV_SendDataDma block?)

 

This looks good…

148239_148239.PNGCapture1.PNG

 

zoomed out - not so good:

148240_148240.PNGCapture2.PNG

 

It looks like I could create a ping pong buffer using 2 dma channels per RX and 2 channels per TX like the sample code from is there any demo code for using I2S? , but I'm going to need all 4 dma channels on the MKL17 for my application (1 for SAI/I2S tx, 1 for SAI/I2S rx, 1 for FlexIO/TDM tx, 1 for FlexIO/TDM rx).

 

Edit: To clarify my application, I need to:

- Implement a 4-channel TDM driver using FlexIO

- Forward 2 (L,R) incoming I2S channels to outgoing TDM

- Forward 3 (L, R, Mic) incoming TDM channels to two outgoing I2S channels (one SAI, one FlexIO)

- No processing, just conversion between digital audio standards

 

I'm interested in the viability of this on an MKL17.

 

Thanks,

Jake Jennings

Original Attachment has been moved to: test-sai-i2s-dma.zip

标签 (1)
0 项奖励
回复
5 回复数

1,324 次查看
jacobjennings
Contributor III

To achieve 2x i2s TX, 1x i2s RX, TDM4 TX and TDM4 RX on one chip, I have drawn the following conclusions:

- Most chips have 1 SAI module which supports only 2 channels L/R, 1x RX, 1x TX

- Higher end chips have SAI module that supports left-aligned TDM, but still 1x RX 1x TX

- With basic DMA, for continuous conversion, you must use 2 channels to make a ping-pong buffer

- With enhanced eDMA, you can set up ping-pong buffers with a single eDMA channel

- FlexIO could be used for i2s, but chips with one SAI module AND FlexIO all only have 4 channels of basic DMA (not eDMA) except K8x

- 4 is not enough DMA channels for continuous conversion

- K8x is the only option for this application

Unfortunately, going from a KL17 to a K8x chip is a serious cost increase. Any advice or corrections are welcome.

Thanks,

Jake

0 项奖励
回复

1,324 次查看
egoodii
Senior Contributor III

'K' series parts (even K10) have an SAI with more capable bus modes including MANY analog channels per RX/TX pair in a TDM or AC97 mode.  The DMA to such a channel can be configured to do ALL channel (de-)interleave and double-buffering. For reference, see also:

is there any demo code for using I2S?

BUT unfortunately in that post, my code was made for the 'Ver 1' ('Z') silicon, and the I2S/SAI changed significantly going into V2 silicon, so the setup of that interface is NOT going to directly apply to current devices...

0 项奖励
回复

1,324 次查看
jacobjennings
Contributor III

The TDM support in K series is nice, but I need to run 2X TDM and 3X I2S (1 rx 2 tx) simultaneously which does not seem possible until K8x

0 项奖励
回复

1,324 次查看
jacobjennings
Contributor III

The ADAU1761 DSP I am using only has one set of digital TX/RX, which is why I wanted to do I2S <-> TDM4 conversions to interface with several I2S-only components. I think it will be better to switch to the TI C5000 series DSP instead of using the main MCU as a converter.

0 项奖励
回复

1,324 次查看
jacobjennings
Contributor III

My mistake: Although most K series have 1 SAI module, some of them support multiple RX/TX lines while sharing clock lines, such as K24, K64

0 项奖励
回复