Re: CodeWarrior MCU V10.3 - PE Support for MK40DX256VMC7 121MAPBGA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: CodeWarrior MCU V10.3 - PE Support for MK40DX256VMC7 121MAPBGA

628 Views
lategoodbye
Senior Contributor I

Hi,

i have nearly the same problem as ride. I want to use the MK20DX256VMC7 (MAPBGA, 121 pin) in CodeWarrior 10.3, but this variant is also unavailable in Processor Expert.

Which variant would be the closest fit?

Is there any way to add support manually for CodeWarrior?

Are there any plans to add 121-MAPBGA packages in the next MCUs Driver Suite for Processor Expert?

Thanks in advance.

0 Kudos
Reply
2 Replies

483 Views
JimDon
Senior Contributor III

You should ask this in the Processor Expert Software forum.

Other than the picture, I don't know that the package effects the code generation.

0 Kudos
Reply

483 Views
lategoodbye
Senior Contributor I

Hi Jim, i started a new discussion in the PE forum. Sure the package had a great influence on code generation, because the available variants have less pins than 121.

0 Kudos
Reply