I am current user of Codewarrior (V10.6) with MQX V4.2 based applications running on a number of K60-based custom boards we have developed.
We are looking to a possible move to K53-based solutions - as these parts seem more available.
Should we also be considering a move to MCUXpresso as the development suite of choice or can we continue using codewarrior for migrating the software to the K53 MCU...?
Also, It looks like there are a number of SDKs available. I'm not sure how these fit into the development environment...Could someone offer some direction..?
thanks
已解决! 转到解答。
Hi @MWMinor
I'm Miguel and I will give support to your case.
You will not have any problem if you migrate from de K60 to the K53. If your applications need CodeWarrior, this IDE supports both boards.
However, I highly recommend you to update your workspace to MCUXpresso since you will have a newer alternative to MQX with FreeRTOS, more information and long term support with this newer IDE.
Best Regards, Miguel.
Hi Miguel
Many thanks for your prompt reply.
I have started the process of migrating one of our K60 projects to a K53-based solution but downloading the MCUexpresso IDE. We have also purchased a TWR-K53N512 development board. When I tried to use the MXUexpresso SDK builder, I could not find the TWR-K53N512 in the list of boards.
How do I build the SDK for the TWR-K53N512 board....?
Thanks
Ken
Hi Miguel
When I searched for the MK53DN512, the system found the TWR-K60D100M board which is slightly confusing.
Can I use this board as an alternative...? ie to get the examples..??
Or am I searching in the wrong place...?
Regards
MWM
Hi @MWMinor
After you dowload the SDK, you will find the examples in the compressed file, these are the same examples as de K60. The location of the examples is SDK_2_2_0_MK53DN512xxx10\boards\twrk60d100m
Let me know if you find them.
Miguel.
Hi Miguel
I found the example programmes for the TER-K60 board within the K53 SDK - but when I tried to run them, they do not all work. For example the RTC test and benchmark tests run ok - I am ssuming this is because the core of the processors is the same - but tests like the GPIO and ADC tests do not work - and I think this is because the IO configuration for the TWR-K60 board is different to the TWR-K53. Is that correct..?
Are there any example projects specifically written for the TWR-K53 board...?
or
Do I have to modify the TWR-K60 projects before they will run on the TWR-K53 board...?
Maybe I am still not looking in the right place for the examples...???
Thanks
Ken