Minnimum Erase size for PFLASH using C90TFS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Minnimum Erase size for PFLASH using C90TFS

ソリューションへジャンプ
3,420件の閲覧回数
sebasira
Senior Contributor I

Hi all!

I'm using routines from C90TFS and working with TWRK60... I'd like to know what's the smaller size I can erase of the PFlash.... The routine FlashEraseSector has destination and size as parameters. Could I especify a word-aligned destination and size=4 and only erase those 4bytes since the destiantion address and leave all the rest of sector untouched?

Best Regards,

SebaS

ラベル(1)
0 件の賞賛
返信
1 解決策
3,006件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

The sector size is the minimal size for erase operation, and it depends on the device, as I know, for K20 50MHz part, it is 1Kbytes/sector, for K60 100MHz part, it is 2Kbyte/sector. so there is no smaller size for this api, the size parameter here should be sector aligned, otherwise an error code FTFx_ERR_SIZE would be returned.

Hope that helps,

元の投稿で解決策を見る

6 返答(返信)
3,007件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

The sector size is the minimal size for erase operation, and it depends on the device, as I know, for K20 50MHz part, it is 1Kbytes/sector, for K60 100MHz part, it is 2Kbyte/sector. so there is no smaller size for this api, the size parameter here should be sector aligned, otherwise an error code FTFx_ERR_SIZE would be returned.

Hope that helps,

3,006件の閲覧回数
sebasira
Senior Contributor I

Thanks for clarify me.

I assume it was as you said, but the size parameter would be meaningless... Why passing an unnecesary parameter that would not only confuse but also return an error?

SebaS

0 件の賞賛
返信
3,006件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

The size parameter is used to specify how many sectors are going be to erased, for example, if the sector size is 2K, and the possible size parameter could be 2K, 4K, 6K and so on. The API would check whether the size parameter is sector aligned, and determine how many sectors to be erased. so this parameter is not needed by FTFL module, but the driver code. Please refer to the following for details.

a1.JPG

Hope that helps,

3,006件の閲覧回数
sebasira
Senior Contributor I

Now it make sense!

Thank you Kan Li!

Best Regards,

SebaS

0 件の賞賛
返信
3,006件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi SebaS,

You are welcome!! Please kindly let me know when you have any issue.

Have a nice day!!

Best Regards,

Kan Li

Technical Information & Commercial Support AP (Kinetis/ColdFire)

Freescale Semiconductor (China) Limited Shanghai Branch Office

0 件の賞賛
返信
3,006件の閲覧回数
GowrishankarChi
NXP Employee
NXP Employee

Seba, send your question to stephenmcginty if he is unable to answer, at least he would know who can....

Message was edited by: Monica Arvizu

0 件の賞賛
返信