Hi I`m thinking of using the MK66FN2M0VLQ18 in a project and need to add SDRAM but I`m a bit confused as I cannot find any examples. It seems that Databus 0 - 15 is not available on FB_AD0-15 as it is used for the address lines - Do I need to use latches to multiplex the data bus with the address lines?
Any help would be greatly appreciated
已解决! 转到解答。
Hi,
I have checked the data sheet of MT48LC8M16A2 – 2 Meg x 16 x 4 Banks, this is the parameters:
row addressing:4K A[11:0]
column addressing:512 A[8:0]
bank addressing:4 BA[1:0]
You have to use the Table 35-8. SDRAM Controller to SDRAM Interface (16-Bit Port, 9-Column Address Lines) in RM of K66, the data bus is hooked to the High half word, I think your connection is okay. but I do not check the pin assignment.
BR
Xiangjun Rong
Hi, Daniel,
Regarding your question, i am a bit confused, do you interface with SDRAM or SRAM? if you hook SDRAM, you have to use SDRAM SDR controller to connect, if you use SRAM/Nor flash, you can use FlexBus to connect.
If you use SDRAM, pls refer to the follwoing table in reference manual of K66.
Pls tell us the device even part number you want to hook.
BR
XiangJun Rong
Hi XiangJun
Thanks for your reply.
The SDRAM is MT48LC8M16A2P-75 (2 Meg x 16 x 4 Banks) - I have attached the pin mapping to what I think may work?
MK66 Pin (LQFP) | MK66 Pin Name | MK66 mode | MT48LC8M16A2P pin | MT48LC8M16A2P pin NAME | |
81 | PTB0 | SDRAM_CAS_b | 17 | SDRAM_CAS | |
82 | PTB1 | SDRAM_RAS_b | 18 | SDRAM_RAS | |
83 | PTB2 | SDRAM_WE | 16 | SDRAM_WE | |
84 | PTB3 | SDRAM_CS0_b | 19 | SDRAM_CS0 | |
106 | PTC3 | CLKOUT | 38 | SDRAM_CLOCKOUT | |
125 | PTC18 | SDRAM_DQM1 | 39 | SDRAM_DQM1 | |
126 | PTC19 | SDRAM_DQM0 | 15 | SDRAM_DQM0 | |
136 | PTD7 | SDRAM_CKE | 37 | SDRAM_CKE | |
96 | PTB17 | FB_AD16/ SDRAM_D16 | 2 | SDRAM_D0 | |
95 | PTB16 | FB_AD17/ SDRAM_D17 | 4 | SDRAM_D1 | |
92 | PTB11 | FB_AD18/ SDRAM_D18 | 5 | SDRAM_D2 | |
91 | PTB10 | FB_AD19/ SDRAM_D19 | 7 | SDRAM_D3 | |
90 | PTB9 | FB_AD20/ SDRAM_D20 | 8 | SDRAM_D4 | |
89 | PTB8 | FB_AD21/ SDRAM_D21 | 10 | SDRAM_D5 | |
88 | PTB7 | FB_AD22/ SDRAM_D22 | 11 | SDRAM_D6 | |
87 | PTB6 | FB_AD23/ SDRAM_D23 | 13 | SDRAM_D7 | |
120 | PTC15 | FB_AD24/ SDRAM_D24 | 42 | SDRAM_D8 | |
119 | PTC14 | FB_AD25/ SDRAM_D25 | 44 | SDRAM_D9 | |
118 | PTC13 | FB_AD26/ SDRAM_D26 | 45 | SDRAM_D10 | |
117 | PTC12 | FB_AD27/ SDRAM_D27 | 47 | SDRAM_D11 | |
102 | PTB23 | FB_AD28/ SDRAM_D28 | 48 | SDRAM_D12 | |
101 | PTB22 | FB_AD29/ SDRAM_D29 | 50 | SDRAM_D13 | |
100 | PTB21 | FB_AD30/ SDRAM_D30 | 51 | SDRAM_D14 | |
99 | PTB20 | FB_AD31/ SDRAM_D31 | 53 | SDRAM_D15 | |
132 | PTD5 | FB_AD1/ SDRAM_A9 | 32 | A7 | |
131 | PTD4 | FB_AD2/ SDRAM_A10 | 31 | A6 | |
130 | PTD3 | FB_AD3/ SDRAM_A11 | 30 | A5 | |
129 | PTD2 | FB_AD4/ SDRAM_A12 | 29 | A4 | |
115 | PTC10 | FB_AD5/ SDRAM_A13 | 26 | A3 | |
114 | PTC9 | FB_AD6/ SDRAM_A14 | 25 | A2 | |
113 | PTC8 | FB_AD7/ SDRAM_A15 | 24 | A1 | |
112 | PTC7 | FB_AD8/ SDRAM_A16 | 23 | A0 | |
110 | PTC5 | FB_AD10/ SDRAM_A18 | 33 | A8 | |
109 | PTC4 | FB_AD11/ SDRAM_A19 | 34 | A9 | |
105 | PTC2 | FB_AD12/ SDRAM_A20 | 22 | A10 | |
104 | PTC1 | FB_AD13/ SDRAM_A21 | 35 | A11 | |
103 | PTC0 | FB_AD14/ SDRAM_A22 | 20 | BANK SEL 0 | |
97 | PTB18 | FB_AD15/ SDRAM_A23 | 21 | BANK SEL 1 |
When using 16-bit wide SDRAM and D16-D31 on the MCU (mandatory from what I understand), is this realy correct:
125 | PTC18 | SDRAM_DQM1 | 39 | SDRAM_DQM1 | |
126 | PTC19 | SDRAM_DQM0 | 15 | SDRAM_DQM0 |
I thought one should connect MCU DQM3 and DQM2 to SDRAM DQM1 and DQM0, or?
Yes I`m pretty sure its correct, I have to admit the datasheet is pretty poor at explaining how to wire SDRAM but the tables 35-4 to 13 are correct so you can blindly follow them. We invited a NXP technical expert to our business to double check for us and he confirmed that the above wiring is correct. The Prototype boards are being made next week so I`ll be pretty disappointed if they don`t work.
Hi Daniel,
I am working with K65, but the Reference manual looks the same. We are about to order a board any day. What I have been looking at is "Figure 35-2. Connections for External Memory Port Sizes" and from that figure my conclusion is that BS3 and BS2 shall be used with 16-bit wide memory (BS[3:0] is the DQM, see table 35-2). You can also check this thread on the same topic: https://community.nxp.com/thread/437787
Hi
I am so confused - I think you are right BS3 and BS2 should be used with 16bit SDRAM but as it is memory mapped does it matter?
Bank select and DQM are two separate items.
Synchronous dynamic random-access memory - Wikipedia
SDRAM devices are internally divided into either 2, 4 or 8 independent internal data banks. One to three Bank Address inputs (BA0, BA1 and BA2) are used to select which bank a command is directed toward.
I`m pretty sure that you can wire the bank select lines straight to the next available address lines.
When checking table 35-2 BS[3:0] should be interpret as "Byte Select" and not "Bank Selection":
"SDRAM byte selects BS[3:0] function as byte enables to the SDRAMs. They connect to the DQM signals (or data qualifier masks) of the SDRAMs.".
In Figure 35-2 the BS signals have the text "Byte Enable" to the left of them to make it more confusing.
A problem is that NXP uses BS instead of DQM in the Reference manual and DQM in the Datasheet not BS.
I am still not 100% sure what is right, but I whould really like be 100% sure before we order our board...
Hi I have contact NXP and they kindly reviewed the design for me, it looks like the design was wrong and that the DQM signals need to connect to DQM2 and DQM3.
Also just to clarify the Bank address lines are correct:
In terms of the Bank Address lines, on the SDR these select one of the 4 internal banks. To make the memory space mapped to the K66 contiguous, we use the next 2 address lines. So I’m happy with using SDRAM_A22 and SDRAM_A23 connected to BANK_SEL0 and BANK_SEL1. That is consistent with both the TWR schematic and the Table 35-16 example in the device reference manual (pdf page 900) of Rev2 reference manual.
So with reasonable confidence below is how you connect 128Mbit of SDRAM to the MK66 in 16bit mode, although we will only 100% know once we have re-spun the PCB.
Connecting MT48LC8M16A2P to MK66FN2M0VLQ18.
MK66 Pin (LQFP) | MK66 Pin Name | MK66 mode | MT48LC8M16A2P pin | MT48LC8M16A2P pin NAME | |
81 | PTB0 | SDRAM_CAS_b | 17 | SDRAM_CAS | |
82 | PTB1 | SDRAM_RAS_b | 18 | SDRAM_RAS | |
83 | PTB2 | SDRAM_WE | 16 | SDRAM_WE | |
84 | PTB3 | SDRAM_CS0_b | 19 | SDRAM_CS0 | |
106 | PTC3 | CLKOUT | 38 | SDRAM_CLOCKOUT | |
124 | PTC17 | SDRAM_DQM3 | 39 | SDRAM_DQMU | |
123 | PTC16 | SDRAM_DQM2 | 15 | SDRAM_DQML | |
136 | PTD7 | SDRAM_CKE | 37 | SDRAM_CKE | |
96 | PTB17 | FB_AD16/ SDRAM_D16 | 2 | SDRAM_D0 | |
95 | PTB16 | FB_AD17/ SDRAM_D17 | 4 | SDRAM_D1 | |
92 | PTB11 | FB_AD18/ SDRAM_D18 | 5 | SDRAM_D2 | |
91 | PTB10 | FB_AD19/ SDRAM_D19 | 7 | SDRAM_D3 | |
90 | PTB9 | FB_AD20/ SDRAM_D20 | 8 | SDRAM_D4 | |
89 | PTB8 | FB_AD21/ SDRAM_D21 | 10 | SDRAM_D5 | |
88 | PTB7 | FB_AD22/ SDRAM_D22 | 11 | SDRAM_D6 | |
87 | PTB6 | FB_AD23/ SDRAM_D23 | 13 | SDRAM_D7 | |
120 | PTC15 | FB_AD24/ SDRAM_D24 | 42 | SDRAM_D8 | |
119 | PTC14 | FB_AD25/ SDRAM_D25 | 44 | SDRAM_D9 | |
118 | PTC13 | FB_AD26/ SDRAM_D26 | 45 | SDRAM_D10 | |
117 | PTC12 | FB_AD27/ SDRAM_D27 | 47 | SDRAM_D11 | |
102 | PTB23 | FB_AD28/ SDRAM_D28 | 48 | SDRAM_D12 | |
101 | PTB22 | FB_AD29/ SDRAM_D29 | 50 | SDRAM_D13 | |
100 | PTB21 | FB_AD30/ SDRAM_D30 | 51 | SDRAM_D14 | |
99 | PTB20 | FB_AD31/ SDRAM_D31 | 53 | SDRAM_D15 | |
132 | PTD5 | FB_AD1/ SDRAM_A9 | 32 | A7 | |
131 | PTD4 | FB_AD2/ SDRAM_A10 | 31 | A6 | |
130 | PTD3 | FB_AD3/ SDRAM_A11 | 30 | A5 | |
129 | PTD2 | FB_AD4/ SDRAM_A12 | 29 | A4 | |
115 | PTC10 | FB_AD5/ SDRAM_A13 | 26 | A3 | |
114 | PTC9 | FB_AD6/ SDRAM_A14 | 25 | A2 | |
113 | PTC8 | FB_AD7/ SDRAM_A15 | 24 | A1 | |
112 | PTC7 | FB_AD8/ SDRAM_A16 | 23 | A0 | |
110 | PTC5 | FB_AD10/ SDRAM_A18 | 33 | A8 | |
109 | PTC4 | FB_AD11/ SDRAM_A19 | 34 | A9 | |
105 | PTC2 | FB_AD12/ SDRAM_A20 | 22 | A10 | |
104 | PTC1 | FB_AD13/ SDRAM_A21 | 35 | A11 | |
103 | PTC0 | FB_AD14/ SDRAM_A22 | 20 | BANK SEL 0 | |
97 | PTB18 | FB_AD15/ SDRAM_A23 | 21 | BANK SEL 1 |
Regards Dan.
Hi,
I have checked the data sheet of MT48LC8M16A2 – 2 Meg x 16 x 4 Banks, this is the parameters:
row addressing:4K A[11:0]
column addressing:512 A[8:0]
bank addressing:4 BA[1:0]
You have to use the Table 35-8. SDRAM Controller to SDRAM Interface (16-Bit Port, 9-Column Address Lines) in RM of K66, the data bus is hooked to the High half word, I think your connection is okay. but I do not check the pin assignment.
BR
Xiangjun Rong
Hi,
For K66, you can locate the SDRAM to the address space:
0x8000_0000–0x8FFF_FFFF SDRAM (External RAM - Write-through) All masters
in other words, your SRDAM space will be:
0x8000 0000 to 0x80FF FFFF for MT48LC8M16A2
But you have to initialize the SDRAM controller before you access the SDRAM.
I attach an doc, hope it can help you.
BR
XiangJun Rong