MCUXpresso Config Tools not working for KW37/38/39 SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso Config Tools not working for KW37/38/39 SDK

826件の閲覧回数
m3
Contributor II

Is there actually any way to configure a SDK(2.6.9) for the KW38? I tried every possilbe SDK version, downloaded from inside and outside the MCUXpresso but none of them will work with the MCUX Config Tools.

 

 

0 件の賞賛
返信
1 返信

815件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

You can refer this topic.

https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpresso-Config-tools-not-opening-for-FRDM-KW38-Board-...

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信