When I try to access the UART0 (and other) registers i am ending up with a hardfault. I am in privileged mode as you can see in the next log from the debugger
Any idea what can be wrong here?
Halting target CPU...
...Target halted (PC = 0x000004E8)
Read 2 bytes @ address 0x000016F6 (Data = 0xF000)
Read 2 bytes @ address 0x000016F6 (Data = 0xF000)
Read 2 bytes @ address 0x000016F6 (Data = 0xF000)
R0 = 00000050, R1 = F000300C, R2 = 00000C00, R3 = 00001800
R4 = 1FFFF348, R5 = FFFFFFFF, R6 = 00000000, R7 = 1FFFF161
R8 = 2BFF2EBF, R9 = B745DFDD, R10= 1FFF3000, R11= 00000000
R12= A6F97FFE, R13= 20003000, MSP= 20003000, PSP= EB7FF6E4
R14(LR) = 1FFFF159, R15(PC) = 000004E8
XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000
CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00
Reading all registers
Read 4 bytes @ address 0x000004E8 (Data = 0xF001B672)
Setting breakpoint @ address 0x0000164A, Size = 2, BPHandle = 0x0001
Setting breakpoint @ address 0x000016EC, Size = 2, BPHandle = 0x0002
Setting breakpoint @ address 0x000016F6, Size = 2, BPHandle = 0x0000
WARNING: No more breakpoint resources left
Starting target CPU...
...Breakpoint reached @ address 0x0000164A
Reading all registers
Removing breakpoint @ address 0x0000164A, Size = 2
Removing breakpoint @ address 0x000016EC, Size = 2
Removing breakpoint @ address 0x000016F6, Size = 2
WARNING: Breakpoint @ address 0x000016F6 not found
Read 4 bytes @ address 0x0000164A (Data = 0x22004B22)
Reading 64 bytes @ address 0x20002FC0
Read 4 bytes @ address 0x00001714 (Data = 0x607B2300)
Read 4 bytes @ address 0x1FFFF000 (Data = 0x01312D00)
Reading 8 bytes @ address 0x1FFFF090
WARNING: Failed to read memory @ address 0x4006A000
Reading 384 bytes @ address 0x4006B000
WARNING: Failed to read memory @ address 0x4006B000
Solved! Go to Solution.
Hi Johan,
Usually hard fault occurs when you try to access a peripheral register without first enabling the clock to the peripheral module from within the SIM module SCGCx registers. The SIM->SCGC4 bit 10 needs to be set to "1" to enable clocking to UART0.
Regards,
David
Hello Johan,
In addition, what software application are you exactly using? I would recommend you to use any of the code examples included in KW0x Board support package as reference. You could download it from “Software & Tools” tab in http://www.freescale.com/kw01.
Regards,
AngelC
Hi Angel,
Found tit yesterday evening and your answer was correct. Some part are a bit confusing regarding the clocking. There are 2 clock registers for the uart bit 10 of SIM_SGC4 and bits 26-27 of SIM_SOPT2 -> defaulted to 0 what means disable.
Apparently only the SIM_SGC4 must be enabled to be able to change the UART register settings even if the UART clock source in SIM_SOPT2 is disabled
I don't use any libraries, we are writing our own to be able to optimize for size and speed
Regards
Johan
Hi Johan,
Usually hard fault occurs when you try to access a peripheral register without first enabling the clock to the peripheral module from within the SIM module SCGCx registers. The SIM->SCGC4 bit 10 needs to be set to "1" to enable clocking to UART0.
Regards,
David