K60 power supply solution

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 power supply solution

跳至解决方案
784 次查看
markoseverin
Contributor II

Hi guys,

I'm making a K60, TQFP144 board with ethernet, SD card and a whole lot of other stuff that uses 3.3V. I need to power the MCU from a 12V battery (let's say range 10 - 14.4V). Most of the time, board will be in power down mode, where I would like to have the power consumption under 100uA. The board needs to be able to wake-up by it self regularly (let's say a few times a day). My problem is designing a power supply for the MCU.

In very low leakage modes the MCU burns a few uA, so that would suggest a low power LDO from 12V to 3.3V. But at run mode, it can consume about 100mA, which is too much for any low power LDO, hence a buck converter should be used. I could use both, but switching between the two would not be easy. I could use a buck and a LDO and two diodes, but that would make the 3.3V line poorly regulated; and I don't want that. A solution is also to use an auxilary KL05 MCU , powered by a LDO, to turn on the buck converter for the K60, but that kinda complicates things too much.

Can anyone suggest a power supply solution for my situation?

Thanks in advance

Marko

标记 (4)
0 项奖励
回复
1 解答
631 次查看
Paul_Tian
NXP Employee
NXP Employee


According to your both low power consume and large current output requirement, I suugest one LDO for your reference. Part number is S-1122B33MC. You can download its datasheet from www.alldatasheet.com

在原帖中查看解决方案

0 项奖励
回复
2 回复数
631 次查看
Monica
Senior Contributor III

Hello Marko,

Please let us know if that was helpful, we'd like to know :smileywink:

Best regards,

Monica.

0 项奖励
回复
632 次查看
Paul_Tian
NXP Employee
NXP Employee


According to your both low power consume and large current output requirement, I suugest one LDO for your reference. Part number is S-1122B33MC. You can download its datasheet from www.alldatasheet.com

0 项奖励
回复