Hello community. just received a kwikstik-40 and am unable to charge the battery

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hello community. just received a kwikstik-40 and am unable to charge the battery

479 次查看
jeffpurcell
Contributor I

Hello community.  just received a kwikstik-40 and am unable to charge the battery via USB. It powers up and runs while connected to USB but even after 5 hours it only shows 1 bar of charge and not enough to power up on the battery.

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

399 次查看
Paul_Tian
NXP Employee
NXP Employee

Hi, Jeff

As you can find, there is a ON/OFF switch on another side of Kwikstik_K40. Did you turn it on when you want to use this board?

If yes, there is still no 3.3V power. I think you need to check if battery still has energy.

Hope my reply can help you. Thanks.

Best Regards

Paul

0 项奖励
回复