HELP WITH THE USE OF THE ADC, KL25N128VLH

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

HELP WITH THE USE OF THE ADC, KL25N128VLH

Jump to solution
927 Views
charlesdiogoama
Contributor II

Good morning,

I am a designer of electronic "Electronics Industry VLP" and am in the midst of developing a project to an HMI (Human Machine Interface) and got in trouble "C" for the use of the ADC.

I'm using a uControlador KL25Z128VLH, King uses all ports ADC ...
however I am not getting even one call.


I appreciate anyone who can help me.
Thank you.

Labels (1)
1 Solution
771 Views
charlesdiogoama
Contributor II

Thank you sir Hui_Ma

I discovered it was just a syntax error,

all settled.

View solution in original post

0 Kudos
Reply
3 Replies
771 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is KL25 ADC example demo located in TWR-KL25DEMO project of KL25_SC file.

You can download KL25_SC software from below link:

http://cache.freescale.com/files/32bit/software/KL25_SC.exe

Wish it helps.

771 Views
charlesdiogoama
Contributor II

Thank you sir kkk

Managed to do the ADC reading however now another problem arises ...

how I can configure the interrupt after the reading is completed?

remembering NOT used the Processor Expert nor MQX ...

0 Kudos
Reply
772 Views
charlesdiogoama
Contributor II

Thank you sir Hui_Ma

I discovered it was just a syntax error,

all settled.

0 Kudos
Reply