FreeMASTER 1.4 Driverless connection using KL25z and OSDA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FreeMASTER 1.4 Driverless connection using KL25z and OSDA

FreeMASTER 1.4 Driverless connection using KL25z and OSDA

There is new amazing feature in FreeMaster ver 1.4 ( www.freescale.com/freemaster ) - you can do the debugging and visualization of your application in FreeMASTER without adding any code in there (you do not need a serial driver of any kind to achieve the connection), just using the communication plug-in to OSDA embedded in new version of Freemaster connected instead of the debugger from IDE.

The driverless use of Freemaster use is easy to use, just open the FreeMaster, assuming you have your own application, without any Freemaster driver in it. Load the application into flash memory of the KL device and close debugging session from IDE.

Open FreeMaster and  go to Project/Options/Comm, use setup from picture below

Choose Plug-in - use the FreeMASTER BDM Communication Plug-in, hit configure and take P&E Kinetis.

OSDA_direct_connection.PNG

you can test the connection there too.

The next step is to go to Options/MAP files, navigate to *.ELF file of your project and set file format to ELF/DWARF (I have chosen .elf from some usb demo project just to show the way how to do so)

map_choice.PNG

well, the connection is established, now there is need to choose variables for display and visualization.

Go to project/Variables and choose variables you want to follow (hit Generate.. to do so, list of variables available in your project will appear and you can choose the desired one and hit generate - it will check and generate the variable connection, you can do it for single variable, array or more variables - it is intuitive )

variable FMSTR.PNG

When desired variables are generated, close the dialog.

You can make a scope or add variables to watch.

To add variable to variable watch window click by right mouse button in watch area

watch_fmstr.png

go to watch properties, Watch tab and hit Add---->> to add it between watched wariables and hit OK

watched var fmstr.PNG

and value appears in the Variable Watch window.

To create scope, go to project tree window and use right mouse button on NewProject, choose Create Scope...

scope.png

In scope properties chose the name for this scope and go to  Setup tab. You can add your variable to the scope here by choosing in drop down menu

scopeProp.png

Hit OK and start the session (Ctrl+K) or hitting Stop icon in the menu, the variable is displayed in the window.

scopewin.PNG

The value in my case stays 0 however displays correctly...

Pavel

评论

Hi Pavel,

this is a great write up!!!!

for some reason I had to reinstall FreeMASTER to see the BDM module, but now it works perfect with my application without any modification!!

This is a such a great tool!!

Please dome more write-ups on what we can do with this: it seems there is so much potential!!!

Thank you very much.

Andrea

hi Pavel,

Thanks for sharing. It is very convenient to use FreeMaster without driver or additional code. Does the driverless use of FreeMaster also apply for the FreeMaster "recorder"?

I've tried to use "BDM JTAG/EOnCE communication plug-in (56F8xxx)" but without success. Is there any special steps need to be followed to use this plug-in for dsc chip (using USBTap).

Thanks,

Jack

Hi Jack

the plugin for DSC JTAG is not working so independent as S08 BDM / Kinetis OSDA plugin, you need to apply small portion of code into the MCU to get it working.

I would recomend you to use Processor Expert to apply the Freemaster into the project, it is intuitive with little guidance from the manual of FreeMaster.

in the configuration of the Freemaster you can easily enable the recorder including setup of its buffers

Pavel

Hi Pavel,

Thanks for your sharing . I want to use FreeMaster  to observe variables in S12x board with BDM module.  But is doesn't work very well. I can't find any examples for this situation. I need your help. Hope your reply!

Sherry

Hi Sherry,

the FreeMaster communication Plug-in should work with HCS08/12. What does it mean doesn't work well? Be sure you have closed the debugging session over BDM

I would recommend to do the test of your Multilink connection / after configuration.

so

in the Project / Options tab where you have selected the Plug-in hit configure button, the cable settings window opens and you are ready to select BDM cable settings to P&E HCS12(z), connection and target, then do the test by hitting Test Connection.

then you should return back to Options and select the MAP Files tab, there you need to apply your elf/abs file and the file format - most likely  should be binary ELF with DWARF debugging info.

choose your desired variables in Project/Variables tab, hit button Generate and select variables you want to work with (arrays or single variables in various formats)

that is the configuration, nothing else

next is to visualize the variables in the Variable watch area-

hit right mouse button in that area, you are allowed to open watch properties, there are 3 boxes, the one in the middle allows you to move from available vars (those you have previously selected in Generate) to Watched vars, Added variables will appear in the Variable Watch area

to see the graphical output, you need to hit New Project using right mouse button in project tree (left upper corner). Choose create scope, set Name and period and link variables from the popup menu below the Graph vars list with Graph vars in Setup tab.

by hitting STOP sign button in the menu you can start the communication, variables listed in Variable watch area should update periodically and once you open the graph it should show the changing (or static) value of the variable in graphical view....

hope I did not miss anything

Pavel

Hi Paval,

I am gratefuI  to hear from you!  Thank you so much to help me . However, I configured the Freemaster as your suggestion,but there existed a situation. When I hit the STOP sign button ,a dialog box then pops up and says  "Contacting the communication" . So I want to know the reason,and how can I solve the problem. Hope your reply!

Hi Sherry

are you using the correct plug in?

was the test of the  communication successful during the configuration?

Pavel

Hi paval,

Thank you so much for your help. Now I am proficient in use of Freemaster to observe the variables. You help me a lot .Thank you again!

Sherry

Hi Pavel,

How are you?

I am doing a project using KL25Z with CodeWarrior 10.6 and NXP KTY82/100 Temperature Sensor for temperature monitoring and measurements. I need to display temperature profile showing temperature readings versus time on FreeMASTER 1.4.

I followed your article and Installed FreeMASTER 1.4, but was struck as I am using OpenSDA (COM 15) and selected Direct RS232 Communication.

However, your article skipped the section on Direct RS232 Communication, but just showed the plug-in Module for FreeMASTER BDM Communication Plug-in, could you please enlighten me how to do the setting of FreeMASTER 1.4 in using OpenSDA.

Thank you very much for your help.

Best Regards

Hoe Min

Hi Paval,

Oops! I forgot to inform you that I am using CodeWarrior 10.6 without Processor Expert.

I am connecting KTY82/100 Temperature Sensor Pin 1, 2, and 3 directly to Pin 12 - GND (Ground) of J9 I/O Header, Pin 8 - P3V3 (3.3V) of J9 I/O Header and Pin 2 - PTB0 (Signal) of KL25Z respectives.

Would appreciate your reply includes the settings of FreeMASTER the way you did on your article (setting on variables, and other setting, etc.), but on Direct 232 communication using OpenSDA (COM 15).

Thanks.

Best Regards

Hoe Min

Hi Paval,

Just want to let you know that I did try on Options under Communication Tab to select S08 BDM / Kinetis OSDA Plug-In,  but there is no plug-in shown (see screen shots below):

pastedImage_0.png

pastedImage_1.png

Thanks.

Best Regards

Hoe Min

无评分
版本历史
最后更新:
‎01-08-2014 02:17 AM
更新人: